Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum 16*2 LCD getting weird characters
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 34 replies
  • Subscribers 425 subscribers
  • Views 13374 views
  • Users 0 members are here
  • lcd
  • arduino
Related

16*2 LCD getting weird characters

jrcs
jrcs over 10 years ago

Hi all.

 

This is my first post so I hope it is at the right place.

 

I'm working on a project whose objective is to control two ac loads (one ac fan, controlled by phase angle control and one ac motor controlled by a 5V relay) and output to an LCD the room temperature and the % of fan speed.

 

 

The code I wrote seem to work fine without the AC loads connected. I tested it for long periods of time (+12 hours) and everything is ok.

 

The problem is when I connect both (or just one) AC loads, I always end up with my LCD info corrupted like this:

 

image

 

https://1drv.ms/i/s!Ah12lhUG5VG8g9FOhR9Y0ccFTsq2Rg

 

Sometimes past 2 minutes, sometimes past 10 minutes... It's random but it always end up like this.

 

 

I'm guessing it's noise problems due to the loads switching TRIAC/Relay. The TRIAC its connected trough a optocoupler but the relay it's directly connected to the arduino.

 

 

First, I put the lcd.clear() function in my code to "rebuild" the info from time to time but it doesen't work 100% and it's not a "clean" solution for the pourpose.

 

 

The AC loads are connected to the grid but the arduino is powered from my computer's usb port. Already put an EMI filter into AC main input of my loads but no solution.

 

Is there a solution to this problem? Any help?

Sorry for my poor english but I'm a little bit rusty.

 

Regards

  • Sign in to reply
  • Cancel

Top Replies

  • niko.vicencio
    niko.vicencio over 9 years ago +3
    Hi I had the same problem, the lcd showed random characters when the electromechanical relay commutated. I solved this problem, changing the relay by a ssr (Solid state relay). I hope that my answer help…
  • WarrenW
    WarrenW over 10 years ago +2
    How are you driving the relay from the arduino? Direct off the micro or via a transistor? Does the relay have a snubber cap across the coil and a back emf diode? Does the arduino have a filter capacitor…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +2
    Can you please provide a schematic of your setup and also a full picture (Cant see all your connections in the one provided. You can upload them right into this community post. I have done what your describing…
  • dougw
    dougw over 10 years ago in reply to jrcs

    Some fancy systems use a triac to turn on AC - where the triac circuit is designed to only turn on when the voltage is crossing zero - this minimizes turn-on noise.

    Can you use a solid state relay? It should have less spark noise.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jrcs
    jrcs over 10 years ago in reply to dougw

    I have another system running with a MOC3041 with zero-cross detector and it runs like a charm.

     

    I haven't had LCD problems since the capacitor instalation but I get those spikes I posted in the image above. Are they dangerous to the Arduino or they are considered safe?

    I can't use a solid state relay on this project.

     

     

    Thanks for your help

    Regards.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 10 years ago in reply to jrcs

    I've seen lots of chips survive that type of spike, but it may stress them.

    Maybe a zener diode would be fast enough to clamp the spike....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to jrcs

    Joao

    when the relay latches and delatches creates an electric arch

    You're quite correct ... this will happen and does so with capacitive and inductive loads much more than resistive loads.

    This is why relays are de-rated for inductive loads.

     

    If the 0.33 gets you past the problem, then its acceptable.

    Did you have LCD problems 20 mins later or was that how long you ran it for.?

     

    I think dougw is right about using the MOC3041 and triac to drive it.

    This will remove all problems, and if you require a much higher current then use the triac to turn on a 230v relay coil which switches the fan.

    It will switch at zero so the noise should not be present.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • niko.vicencio
    niko.vicencio over 9 years ago

    Hi

     

    I had the same problem, the lcd showed random characters when the electromechanical relay commutated. I solved this problem, changing the relay by a ssr (Solid state relay). I hope that my answer help you.

     

    Nicolás

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 9 years ago in reply to jrcs

    Just filter the power to the low power circuit being affected by the noise (the LCD and arduino)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • D_Hersey
    D_Hersey over 9 years ago

    For a pure inductive load, switching at the zero crossing is stressful on the switch

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • D_Hersey
    D_Hersey over 9 years ago

    http://www.st.com/content/ccc/resource/technical/document/application_note/2f/f7/75/f5/9d/3d/44/04/CD00003867.pdf/files/…

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gurnaldo
    gurnaldo over 7 years ago

    Hi,

    I was facing same problem.

    But I solved it by switching AC inductive loads through 24v relay and also having different power supplies for Arduino and relay and no common ground between them.

    And do use optocoupler to operate the relay.

    Thanks and regards,

    Gurpreet

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • lastnik
    lastnik over 6 years ago in reply to niko.vicencio

    I had the same problem .It works very well. Thanks

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<>