Arduino Forum First project good for begginer
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
  • Replies 6 replies
  • Subscribers 393 subscribers
  • Views 403 views
  • Users 0 members are here
Related

First project good for begginer

Former Member
Former Member over 9 years ago

I am begginer and i bought a kit with this stuff:

1X UNO R3+USB cable;

1X 65PCS/pack BREADBOARD JUMPERS;

1X830 Points HIGH QUALITY BREADBOARD;

15XLED (Red, Green, Yellow);

30X RESISTORS(220R, 10K, 1K);

1X 10 PIN DUPONT LINE(MALE TO FEMALE);

1X Potentiometer;

1X Active Buzzer;

1X Passive Buzzer;

1X 74HC595N;

1X Infrared receiving head;

1X  LM35DZLM35DZ

1X Flame sensor;

1X Roll Ball Switch;

3X 5mm LDR;

5X Button Switch with Cap;

1X IR remote control;

1X Four digital tube;

1X 8*8 Dot Matrix;

1X One digital tube;

1X UNL2003 driver board;

1X Serveo motor

1X 5V Stepper motor;

1X SG90;

1X LCD1602 IIC I2C;

1X PS2 GAME JOYSTICK;

1X DHT11 Digital Temperature and Humidity Sensor;

1X Water level measurement module;

1X RFID module;

1X RFID KEY RING;

1X RFID CARD;

1X SOUND MODULE;

1X 1 ROAD RELAY MODULE;

1X RTC Module;

1X 16 buttons Matrix Keyboard;

1X RGB Three Color Module;

1X 9V Battery Connector.

So i thought,what creative and awesome can i make with this stuff?

 

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago +1
    I would start with the basics BLINK an LED, Without the delay() function Set the millis() onto the LCD display Read the potentiometer and send the value over the serial port Now with a few basics. combine…
  • clem57
    clem57 over 9 years ago

    A very good place to start learning is at Jeremy Blum Arduino Tutorials . He starts off simple and teaches you the fundamentals.
    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 9 years ago in reply to clem57

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 9 years ago

    With those parts, you should be able to explore nearly all of the features of your Arduino.

     

    Check the web, there are plenty of project tutorials for you to work with.

     

    The projects defined by Jeremy Bloom are a good first step to walk you through the capabilities, learn how to code and understand what you should be learning with each project.

     

    What is you end game?  What do you want to do with this capability once you get comfortable working with the pieces?

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago

    I would start with the basics

     

    BLINK an LED, Without the delay() function image

    Set the millis() onto the LCD display

    Read the potentiometer and send the value over the serial port

     

    Now with a few basics. combine the read potentiometer and display to the LCD into one sketch to read the pot and show the ADC value on the LCD

     

    drive the stepper motor

    use the pot to drive the stepper speed and direction

    drive the stepper with the pot and also display current speed and direction on the LCD

     

    basically, take the simple stand alone examples and then build upon them as you learn how each one works

     

    once you have a few basics figured out, you can get to the slightly more complex tutorials I have produced here :- Fast Track to Arduino Programming

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 9 years ago in reply to DAB

    Well i don't know for now.

    I'm currently gonna watch tutorials and then see what next.

    I had an idea of advanced weather station.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 9 years ago in reply to Robert Peter Oakes

    Thank you!

    I will surely check out your tutorial and

    try some basics.