Arduino Forum First project good for begginer
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
  • Replies 6 replies
  • Subscribers 393 subscribers
  • Views 405 views
  • Users 0 members are here
Related

First project good for begginer

Former Member
Former Member over 9 years ago

I am begginer and i bought a kit with this stuff:

1X UNO R3+USB cable;

1X 65PCS/pack BREADBOARD JUMPERS;

1X830 Points HIGH QUALITY BREADBOARD;

15XLED (Red, Green, Yellow);

30X RESISTORS(220R, 10K, 1K);

1X 10 PIN DUPONT LINE(MALE TO FEMALE);

1X Potentiometer;

1X Active Buzzer;

1X Passive Buzzer;

1X 74HC595N;

1X Infrared receiving head;

1X  LM35DZLM35DZ

1X Flame sensor;

1X Roll Ball Switch;

3X 5mm LDR;

5X Button Switch with Cap;

1X IR remote control;

1X Four digital tube;

1X 8*8 Dot Matrix;

1X One digital tube;

1X UNL2003 driver board;

1X Serveo motor

1X 5V Stepper motor;

1X SG90;

1X LCD1602 IIC I2C;

1X PS2 GAME JOYSTICK;

1X DHT11 Digital Temperature and Humidity Sensor;

1X Water level measurement module;

1X RFID module;

1X RFID KEY RING;

1X RFID CARD;

1X SOUND MODULE;

1X 1 ROAD RELAY MODULE;

1X RTC Module;

1X 16 buttons Matrix Keyboard;

1X RGB Three Color Module;

1X 9V Battery Connector.

So i thought,what creative and awesome can i make with this stuff?

 

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago +1
    I would start with the basics BLINK an LED, Without the delay() function Set the millis() onto the LCD display Read the potentiometer and send the value over the serial port Now with a few basics. combine…
Parents
  • clem57
    clem57 over 9 years ago

    A very good place to start learning is at Jeremy Blum Arduino Tutorials . He starts off simple and teaches you the fundamentals.
    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 9 years ago in reply to clem57

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 9 years ago in reply to clem57

    Thanks!