Arduino
  • Products
  • More
Arduino
Arduino Forum How o measure 4-20 mA Current
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 420 subscribers
  • Views 5612 views
  • Users 0 members are here
  • frontpage
Related

How o measure 4-20 mA Current

oksbwn
oksbwn over 10 years ago

I need to measure 4-20mA current output from some sensors. How can i do that ? Currently i use resistive drop to get the analog voltage and provide that to ADC of the controller. Are their any current input ADC ?

  • Sign in to reply
  • Cancel

Top Replies

  • kulky64
    kulky64 over 10 years ago +2
    That's basically how you do it. You can check various manufacturers reference designs, for example: Analog Devices: http://www.analog.com/en/design-center/reference-designs/hardware-reference-design/circuits…
  • uscdadnyc
    uscdadnyc over 10 years ago in reply to oksbwn +2
    Is the situation: (a) Measuring DC Current (at Currents mentioned) AS you would using a (temporary) Test Instrument? OR (b) Circuitry that you would build that attaches to the circuitry that you want to…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +2
    4-20mA is a nice standard for instrumentation measurement and is used in industry extensively. the nice thing about it is it has automatic fault detections as zero = 4mA, any less than 4 means an error…
Parents
  • bhaskar.anil430
    bhaskar.anil430 over 8 years ago

    I wrote this article for reading 4-20mA using Arduino. I am using ADS1115 and INA196 to read the current and convert into digital values.

    feel free to check out.

    https://ncd.io/how-to-read-4-20ma-current-loop-sensors/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • bhaskar.anil430
    bhaskar.anil430 over 8 years ago

    I wrote this article for reading 4-20mA using Arduino. I am using ADS1115 and INA196 to read the current and convert into digital values.

    feel free to check out.

    https://ncd.io/how-to-read-4-20ma-current-loop-sensors/