Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Circuit Review
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 42 replies
  • Subscribers 416 subscribers
  • Views 5321 views
  • Users 0 members are here
Related

Circuit Review

s1buell
s1buell over 8 years ago

  I`m currently making some proto circuits and I would love some feed back/Ideas etc.

 

All these circuits will connect to Arduino or Arduino compatible devices.

 

Anyone have time to help out with some reviews?

 

First circuit is a 4-20ma board

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 8 years ago in reply to s1buell +4
    You might need to modify your 4-20ma loop front end somewhat. First, the circuit as shown does not have a return path for the current loops. Also, the current loop may not necessarily be directly referenced…
  • genebren
    genebren over 8 years ago in reply to s1buell +4
    Tom, Again, I am not sure that you can count on the second leg of the 4-20ma loop to be at ground potential. You might end up shorting out a driver or introducing ground noise into the circuit. Here is…
  • genebren
    genebren over 8 years ago in reply to s1buell +4
    Tom, Here is an even better link. This shows how to differential sense the loop current. https://www.sensorsmag.com/components/implementing-a-4-ma-to-20-ma-sensor-interface Good luck! Gene
Parents
  • s1buell
    s1buell over 8 years ago

    Ok, I`m going to rework the 4-20 area utilizing the LM358. I`ll post the idea later. If you have time can you review this Rs485 circuit? Its intended to connect ModBus type devices.

     

    I added high speed optical separation from the pic to Rs485 chip. I as going to add complete power separation on the RS485 in side but I stopped due to this being a test unit.

     

                                        image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • s1buell
    s1buell over 8 years ago

    Ok, I`m going to rework the 4-20 area utilizing the LM358. I`ll post the idea later. If you have time can you review this Rs485 circuit? Its intended to connect ModBus type devices.

     

    I added high speed optical separation from the pic to Rs485 chip. I as going to add complete power separation on the RS485 in side but I stopped due to this being a test unit.

     

                                        image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • genebren
    genebren over 8 years ago in reply to s1buell

    Tom,

     

    I am not sure that the isolation that you have designed will do anything.  The 485 transceiver will take the hit if anything happens on the bus.  It is extremely unlikely that anything is going to get past the transceiver.  The only way that the opto-isolators would be helpful is if the transceiver was also isolated on a separate power supply (along with the transceiver side of the optos).

     

    What I would do, is attempt to protect the transceiver with a transzorb(s).  One bidirectional transzorb between the A/B pins of the transceiver, along with optional transzorbs from the A/B pins to the power rails.  Also, I would land a resistor pad(s) across the A/B pins with a jumper, to allow the module to be a terminated if it is the end module on the bus (I like this better than placing the terminator at the connector).

     

    Gene