Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Circuit Review
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 42 replies
  • Subscribers 416 subscribers
  • Views 5331 views
  • Users 0 members are here
Related

Circuit Review

s1buell
s1buell over 8 years ago

  I`m currently making some proto circuits and I would love some feed back/Ideas etc.

 

All these circuits will connect to Arduino or Arduino compatible devices.

 

Anyone have time to help out with some reviews?

 

First circuit is a 4-20ma board

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 8 years ago in reply to s1buell +4
    You might need to modify your 4-20ma loop front end somewhat. First, the circuit as shown does not have a return path for the current loops. Also, the current loop may not necessarily be directly referenced…
  • genebren
    genebren over 8 years ago in reply to s1buell +4
    Tom, Again, I am not sure that you can count on the second leg of the 4-20ma loop to be at ground potential. You might end up shorting out a driver or introducing ground noise into the circuit. Here is…
  • genebren
    genebren over 8 years ago in reply to s1buell +4
    Tom, Here is an even better link. This shows how to differential sense the loop current. https://www.sensorsmag.com/components/implementing-a-4-ma-to-20-ma-sensor-interface Good luck! Gene
Parents
  • s1buell
    s1buell over 8 years ago

    RS232 with TVS protection

     

    I used .1uF Tant at 3.3VCD power input. Now the manual says to use a different config but everything I read and every circuit I see is using this config at 3.3VDC.image

     

    Have a look.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • s1buell
    s1buell over 8 years ago

    RS232 with TVS protection

     

    I used .1uF Tant at 3.3VCD power input. Now the manual says to use a different config but everything I read and every circuit I see is using this config at 3.3VDC.image

     

    Have a look.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • genebren
    genebren over 8 years ago in reply to s1buell

    Tom,

     

    Typically the bypass capacitor (in this case C5) does not need to be a tantalum.  I usually just use a ceramic.  Otherwise, this looks good.

     

    Gene