Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Circuit Review
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 42 replies
  • Subscribers 416 subscribers
  • Views 5321 views
  • Users 0 members are here
Related

Circuit Review

s1buell
s1buell over 8 years ago

  I`m currently making some proto circuits and I would love some feed back/Ideas etc.

 

All these circuits will connect to Arduino or Arduino compatible devices.

 

Anyone have time to help out with some reviews?

 

First circuit is a 4-20ma board

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 8 years ago in reply to s1buell +4
    You might need to modify your 4-20ma loop front end somewhat. First, the circuit as shown does not have a return path for the current loops. Also, the current loop may not necessarily be directly referenced…
  • genebren
    genebren over 8 years ago in reply to s1buell +4
    Tom, Again, I am not sure that you can count on the second leg of the 4-20ma loop to be at ground potential. You might end up shorting out a driver or introducing ground noise into the circuit. Here is…
  • genebren
    genebren over 8 years ago in reply to s1buell +4
    Tom, Here is an even better link. This shows how to differential sense the loop current. https://www.sensorsmag.com/components/implementing-a-4-ma-to-20-ma-sensor-interface Good luck! Gene
Parents
  • s1buell
    s1buell over 8 years ago

    image

     

    Does these look right. At 12VDC I used a 16VDC TVS @ 5VDC I used an 8VDC unit

     

    8VDC (Voltage - Reverse Standoff (Typ)

    12VDC Voltage - Reverse Standoff (Typ)

     

    I didn't add the terminator this model is designed to always be the Master. I will add this to the other slave model.

     

    I added the 10ohm 1w resistor as an energy adsorbing resistor, always on the receiving side of the TVS

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 8 years ago in reply to s1buell

    Tom,

     

    This is a little more like what I was talking about:

    image

    This provides line to line and either line to rail protection.  These are bi-directional transzorbs, voltages should be in the VCC range (or slightly less).  The resistor, while normally a good idea, might not be the best way to go with a RS485 transceiver as would imbalance the signal a bit (depending on the terminator value).  The transzorbs are a nice touch, but I know many people do without them and their designs still work.  This is more of a protection against static discharge and gross mis-wiring.

     

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • genebren
    genebren over 8 years ago in reply to s1buell

    Tom,

     

    This is a little more like what I was talking about:

    image

    This provides line to line and either line to rail protection.  These are bi-directional transzorbs, voltages should be in the VCC range (or slightly less).  The resistor, while normally a good idea, might not be the best way to go with a RS485 transceiver as would imbalance the signal a bit (depending on the terminator value).  The transzorbs are a nice touch, but I know many people do without them and their designs still work.  This is more of a protection against static discharge and gross mis-wiring.

     

    Gene