Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Circuit Review
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 42 replies
  • Subscribers 416 subscribers
  • Views 5289 views
  • Users 0 members are here
Related

Circuit Review

s1buell
s1buell over 8 years ago

  I`m currently making some proto circuits and I would love some feed back/Ideas etc.

 

All these circuits will connect to Arduino or Arduino compatible devices.

 

Anyone have time to help out with some reviews?

 

First circuit is a 4-20ma board

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 8 years ago in reply to s1buell +4
    You might need to modify your 4-20ma loop front end somewhat. First, the circuit as shown does not have a return path for the current loops. Also, the current loop may not necessarily be directly referenced…
  • genebren
    genebren over 8 years ago in reply to s1buell +4
    Tom, Again, I am not sure that you can count on the second leg of the 4-20ma loop to be at ground potential. You might end up shorting out a driver or introducing ground noise into the circuit. Here is…
  • genebren
    genebren over 8 years ago in reply to s1buell +4
    Tom, Here is an even better link. This shows how to differential sense the loop current. https://www.sensorsmag.com/components/implementing-a-4-ma-to-20-ma-sensor-interface Good luck! Gene
Parents
  • s1buell
    s1buell over 8 years ago

    Picking the right TVS Diode

     

    Look at the Max Driver Output from here you need to pick a diode that works in the range

     

    Figure 1: MAX3232 Driver Operation Voltage

    image

     

    MAX481CSA+-ND

     

    Driver Input Voltage (DI).............................-0.5V to (VCC+ 0.5V)

    Driver Output Voltage (A, B)...................................-8V to +12.5V

     

    In this case I took the  SMBJ7.0CA-E3/52SMBJ7.0CA-E3/52 as it will cover both circuits(7 to 12VDC

     

    T

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 8 years ago in reply to s1buell

    Tom.

     

    This is a somewhat confusing specification.  The 'Absolute Maximum Ratings' section of a specification is more about the worst possible case or the point were you are most likely going to damage the device.  Typical specifications are usually a better guide as to what range yo want to protect.  If the device you are communicating with is also powered at 5V (not sure if you have stated what Vcc is), it is unlikely that you would see -8 to +12.5V swings.

     

    Gene

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • genebren
    genebren over 8 years ago in reply to s1buell

    Tom.

     

    This is a somewhat confusing specification.  The 'Absolute Maximum Ratings' section of a specification is more about the worst possible case or the point were you are most likely going to damage the device.  Typical specifications are usually a better guide as to what range yo want to protect.  If the device you are communicating with is also powered at 5V (not sure if you have stated what Vcc is), it is unlikely that you would see -8 to +12.5V swings.

     

    Gene

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • s1buell
    s1buell over 8 years ago in reply to genebren

    Yes agree. I reviewed the worst-case spec`s (13VDC upper end for example) and then put the TVS inside these specs to save the components. I really like these TVS diodes they are an easy way to protect bus side of the solution.

    So, do you think its worth keeping the optical chips?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 8 years ago in reply to s1buell

    Tom,

     

    Strange, but I had replied earlier, and stated that I think you should leave out the Optoisolators.  They really are buying you and protection given that the transceiver is now protected nicely.  About the only time I would use the optoisolators is if the transceiver was power by an isolated DC-to-DC supply, or if there was a high voltage source nearby (on the other side of the 485 bus).

     

    Good job!

    Gene