Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Can Arduino Uno R3 board remove chip on the board?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 416 subscribers
  • Views 3361 views
  • Users 0 members are here
  • arduino
Related

Can Arduino Uno R3 board remove chip on the board?

thesea
thesea over 7 years ago

Hello

 

 

First off, got my Elegoo Uno board as Christmas gift, so this is all new to me.

 

 

Here is my problem, I built an motor project and the chip has been programmed. Can I remove the chip from the Uno board?

 

 

Or can I placing a new chip onto the Uno board?

 

 

Best regards.

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 7 years ago +3
    If your board looks like this with the big black ATMega328P in a DIP package, then the chip can be removed: If it looks like this (Arduino Uno R3 SMD) with a small package, it is surface mount and soldered…
  • ralphjy
    ralphjy over 7 years ago +2
    Why is it that you want to replace the chip? If you just want to do a different project, the part can be reprogrammed using a new sketch. And you can always revert back to the motor project as long as…
  • jomoenginer
    jomoenginer over 7 years ago in reply to jomoenginer +2
    This is referenced in the link I provided and shows more detail as to how to build an Arduino on a Breadboard. https://www.arduino.cc/en/Main/Standalone
Parents
  • Gough Lui
    Gough Lui over 7 years ago

    If your board looks like this with the big black ATMega328P in a DIP package, then the chip can be removed:

    image

    If it looks like this (Arduino Uno R3 SMD) with a small package, it is surface mount and soldered to the board, and thus not designed to be removed:

    Image result for arduino uno R3

     

    If you remove the chip, be aware that the chip cannot be used "on its own". The chip needs a clock source at the least - in Arduino, this means having a 16Mhz crystal with two decoupling capacitors to ground.

     

    Also note you cannot just replace the ATMega328P with any other ATMega328P without first burning the bootloader to the chip. The bootloader is a small piece of software that resides on the microcontroller which allows you to reprogram it via serial/USB. Brand new ATMega328P chips are blank (unless someone has programmed the bootloader for you). If you have a few wires and a second Arduino, you can use ArduinoISP to program the bootloader onto a blank chip - but if you don't do this and just insert a blank ATMega328P into your board, you will find you can't program it!

     

    - Gough

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Gough Lui
    Gough Lui over 7 years ago

    If your board looks like this with the big black ATMega328P in a DIP package, then the chip can be removed:

    image

    If it looks like this (Arduino Uno R3 SMD) with a small package, it is surface mount and soldered to the board, and thus not designed to be removed:

    Image result for arduino uno R3

     

    If you remove the chip, be aware that the chip cannot be used "on its own". The chip needs a clock source at the least - in Arduino, this means having a 16Mhz crystal with two decoupling capacitors to ground.

     

    Also note you cannot just replace the ATMega328P with any other ATMega328P without first burning the bootloader to the chip. The bootloader is a small piece of software that resides on the microcontroller which allows you to reprogram it via serial/USB. Brand new ATMega328P chips are blank (unless someone has programmed the bootloader for you). If you have a few wires and a second Arduino, you can use ArduinoISP to program the bootloader onto a blank chip - but if you don't do this and just insert a blank ATMega328P into your board, you will find you can't program it!

     

    - Gough

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • thesea
    thesea over 7 years ago in reply to Gough Lui

    Thank for your information, very useful.