Arduino Forum Complete beginner requiring help with Bluefruit Feather programming
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
  • State Suggested Answer
  • Replies 25 replies
  • Answers 18 answers
  • Subscribers 403 subscribers
  • Views 3789 views
  • Users 0 members are here
Related

Complete beginner requiring help with Bluefruit Feather programming

marks+
marks+ over 6 years ago

Hello, I’m completely new to the Arduino family of PCBs & I have no experience of using them. So I have found myself in at the deep end without a clue!

 

We use Bluefruit Feather PCB nRF52832 for our products. The software we’re using is the official Arduino software.

 

It appears we can plug the boards into the PC via a standard USB lead and program them by opening a “sketch” and select “upload”.

The software compiles the sketches and then attempts to transfer them to the Feather. We then start getting messages saying there are errors or we need to update the bootloader or the boards are not in “DFU”mode.

 

We have tried updating and looked up and tried DFU mode but have had no joy.

 

I believe I may have discovered that our USB cable maybe of the wrong type, so I have another I'm going to be trying in the morning.

I have also downloaded the software on a different laptop to see if that makes a difference.

 

I have no doubt I am doing something incredibly simply wrong but would appreciate some advice on how to proceed.

 

TIA

Mark

  • Sign in to reply
  • Cancel

Top Replies

  • fmilburn
    fmilburn over 6 years ago in reply to marks+ +5 suggested
    I have not used the Nrf Bluefruit feathers so can’t really comment on that. I have used a M0 and M4 express feather without a problem on Windows 10. They both came configured to use Circuit Python if I…
  • cstanton
    cstanton over 6 years ago in reply to marks+ +3 suggested
    marks+ , looks like you're getting two different error messages here. Your error message at https://www.element14.com/community/message/283091/l/re-complete-beginner-requiring-help-with-bluefruit-feather…
  • 14rhb
    14rhb over 6 years ago +2 suggested
    Hi marks+ Just to check, have you selected the correct board under the board manager tab? Looks like you need to set a few things up first as well: https://learn.adafruit.com/bluefruit-nrf52-feather-learning…
  • 14rhb
    0 14rhb over 6 years ago

    Hi marks+

     

    Just to check, have you selected the correct board under the board manager tab?

     

    Looks like you need to set a few things up first as well: https://learn.adafruit.com/bluefruit-nrf52-feather-learning-guide/arduino-bsp-setup

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • marks+
    0 marks+ over 6 years ago in reply to 14rhb

    Hi 14rhb,

    Yes I believe so.

    Also tried three different boards, only one of which was brand new. The other two have been opened and used but their status is unknown.

    I started using them to see if I could manage to do a factory reset and get them working before moving onto a new board.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • marks+
    0 marks+ over 6 years ago in reply to 14rhb

    Thanks for the link. Will give that a try in the morning!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 14rhb
    0 14rhb over 6 years ago in reply to marks+

    There's a slightly hidden link in that one as well for updating the DFU bootloader: the link takes you to https://learn.adafruit.com/bluefruit-nrf52-feather-learning-guide/updating-the-bootloader

     

    Good luck and I'd be interested to hear if you get them working and how you fix them.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • marks+
    0 marks+ over 6 years ago in reply to 14rhb

    cheers, I'll update this thread when I've been able to give everything a try

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • marks+
    0 marks+ over 6 years ago in reply to 14rhb

    Hi

     

    I have updated everything correctly (i think) but I'm getting the following error while updating the bootloader

     

    Error: Invalid value for "-pkg" / "--package": Path "C:\Users\Mark D\Documents\ArduinoData\packages\adafruit\hardware\nrf52\0.14.0/bootloader/feather_nrf52832/feather_nrf52832_bootloader-0.2.13_s132_6.1.1.zip" does not exist.

    Error while burning bootloader.

     

     

    For the record this is the set up I'm trying to use.

    Arduino: 1.8.9 (Windows Store 1.8.21.0) (Windows 10), Board: "Adafruit Bluefruit Feather nRF52832, 0.2.13 SoftDevice s132 6.1.1, Level 0 (Release)"

     

    I have moved onto my home laptop with a different USB lead and I have had a quick go with an Arduino starter kit using an UNO board. I have been successfully tinkering with the blink sketch. So I'm happy my laptop and arduino software is all working as it should. I have remembered to swap over the board names beforehand too. I have then again followed your advice and appear to have everything in place. As it says the bootloader doesn't exist I have downloaded it seperately and copied it into the the correct folder ***0.14.0 BUT it doesn't have the forward slash / part meaning bootloader/feather_nrf52832/

    Do I simply rename the file with the above front it on?

     

    regards

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • 14rhb
    0 14rhb over 6 years ago in reply to marks+

    OK - hopefully fixable image.

     

    My first observation is the space in your path between "Mark" and "D"....often a source of gumbling with OS's. I'd try getting that replaced with a underscore if you can both in your commandline and physically on the filesystem.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • 14rhb
    0 14rhb over 6 years ago in reply to 14rhb

    I must confess I hadn't actually read through those instructions on flashing the boot loader. Options (1) and (3) require the use of a Segger J-Link device which is some expensive hardware. Option (2) appears to allow you to flash the bootloader from Arduino IDE using the nRF5x command line tools from Nordic....I'm assuming that was what you tried?

     

    However reflashing the bootloader is quite drastic so perhaps it is a good job we haven't managed it yet. I'm thinking there may be something far more simple causing these issues.

     

    When I installed the nRF board from the Arduino board manager to see the issues you were facing I noticed there were three different packages available. Perhaps your selected one isn't quite matched to the board still? Some screen shots and a photo of the board might help in identifying the issue. For example any silkscreen id off the board would help as well.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • marks+
    0 marks+ over 6 years ago in reply to 14rhb

    image

    image

     

    I wasn't sure what programmer to select but as I've seen the DFU being mentioned in threads elsewhere I chose that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • 14rhb
    0 14rhb over 6 years ago in reply to marks+

    Your first photo might just be because the board is using a generic USB adapter...could be a red herring.

     

    Please could you post a screenhot of what error(s) you get when attempting to build/upload your sketch?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>