Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Serial device not recognized by zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 372 subscribers
  • Views 1323 views
  • Users 0 members are here
  • zedboardcmty
Related

Serial device not recognized by zedboard

david131
david131 over 6 years ago

Hello!

I need your help, recently I have installed Ubuntu 18.04 on my zedboard but I cannot make work a serial device connected to the USB OTG port. When I connect a pen drive, wireless keyboard or wireless wifi adapter, everything works well, but when I connect a device which must be seen as a "tty", nothing appears. The device is listed with the command "lsusb" but no UART port appears.

 

Do I have to configure something? What am I missing?

 

Thank you very much.

  • Sign in to reply
  • Cancel
Parents
  • drozwood90
    drozwood90 over 6 years ago

    Hi there,

     

    Shooting in the dark - as we do not support Ubuntu - but are you sure there are drivers installed in your OS?  If it is showing up with LSUSB but the port doesn't appear, sounds like a driver issue to me.

     

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • david131
    david131 over 6 years ago in reply to drozwood90

    Yes, maybe there is a problem with drivers but for me is extrange that other USB devices work except which have to use the serial port... I downloaded the ubuntu image from here: https://www.digikey.com/eewiki/display/linuxonarm/Zynq-7000#Zynq-7000-Ubuntu18.04LTS

     

    Thank you!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • drozwood90
    drozwood90 over 6 years ago in reply to david131

    Hi there,


    Thanks for sharing.  That is really interesting.  This has nothing to do with your solution, but since we have had some dealings with Ubuntu under PYNQ, I'm curious, why are you using Ubuntu vs PetaLinux?  I know we used it because of PYNQ.

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • david131
    david131 over 6 years ago in reply to drozwood90

    Only because I already had some code made in Ubuntu with two libraries, gpgme and libcurl, and I didn't know if the program I made would be compatible with petalinux. So Ubuntu was the obvious choice for me.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • david131
    david131 over 6 years ago in reply to drozwood90

    Only because I already had some code made in Ubuntu with two libraries, gpgme and libcurl, and I didn't know if the program I made would be compatible with petalinux. So Ubuntu was the obvious choice for me.