Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Talking to the PHY with MDIO/MDC
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 373 subscribers
  • Views 1690 views
  • Users 0 members are here
  • net1
  • Zedboard Hardware Design
  • ethernet shield
  • fmc carrier card
  • zedboardcmty
Related

Talking to the PHY with MDIO/MDC

andyy
andyy over 6 years ago

Hey, I have a problem with the Phys of the AES-FMC-NETW1-G module. The Phys are not responding to enquirys at the MDIO/MDC interface.

 

The boards are: AES-ZU-PCIECC-G - AES-ZU3EG-1-SOM-I-G - AES-FMC-NETW1-G.

 

Attached you can see that the Phy 1 is not responding:

image

 

Actually I do not know exactly how I can go one. Normally the Phy should speak to me at address 0x01. Some ideas/hints/help for me? Do I need to enable the MDIO/MDC interface at the board?

  • Sign in to reply
  • Cancel
Parents
  • narrucmot
    narrucmot over 6 years ago

    Hi Andyy,

     

    You have mentioned you are using the Avnet UltraZed-EG SOM with PCIe Carrier and NETW1 FMC module, but you haven't mentioned what Vivado hw project and, presumably, what PetaLinux BSP you are using.

     

    Though each Ethernet PHY on the NETW1 FMC has its own MDIO interface, these MDIO interfaces also have to be enabled, along with the associated GEM interface, in the ZU+ Processing System (PS) in Vivado.  For example:

    2072.contentimage_192210.png

     

    By default in the BSP that Avnet posts online for the UltraZed-EG + PCIe Carrier only enables one GEM + MDIO interface.  If you need to enable more GEM + MDIO interfaces you will need to open included Vivado project in the BSP and update the PS configuration to match your needs.

     

    The schematics for the NETW1 FMC can be found here:

    http://www.ultrazed.org/product/network-fmc-module

     

    The PetaLinux BSPs for the UltraZed-EG can be found here:

    https://www.element14.com/community/community/designcenter/zedboardcommunity/ultrazed/ultrazed-eg#e14tab2

     

    --Tom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • andyy
    andyy over 6 years ago in reply to narrucmot

    Hello Tom,

     

    both of the Phys are connected directly to an industrial ethernet real time IP core. Actually there is no GEM involved even the one of the carrier card. There is no Linux. I have run a bare metal driver application at R5.0. The data exchange via real time channel is working. The both Phys are connecting and they transmit/receive data correctly. I need to talk to the management interface for getting the link state and speed...
    Thank you I have the schematics. I'll see the pullup resistor at MDIO line and I was using this for measuring with the probe. I also have the datasheets of the Phy. I can't see anything concerning an init routine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • narrucmot
    narrucmot over 6 years ago in reply to andyy

    It sounds like you are using the Xilinx Time Sensitive Networking IP?  If so, you may have more success with answers to your questions on the Xilinx forums.

    https://forums.xilinx.com/t5/forums/searchpage/tab/message?advanced=false&allow_punctuation=false&q=tsn

     

    If you haven't already, you may want to register for access to the Xilinx TSV IP lounge.  This will give you access to documentation for the TSN IP.

    https://www.xilinx.com/products/intellectual-property/ef-di-25g-tsn-802-1-cm.html#documentation

     

    I suspect the issue you are seeing is that the MDIO interfaces on the PHYs are not connected to the TSN IP inside the Zynq UltraScale+ (ZU+) Programmable Logic (PL).  You will need the Vivado project to determine that.

     

    --Tom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • narrucmot
    narrucmot over 6 years ago in reply to andyy

    It sounds like you are using the Xilinx Time Sensitive Networking IP?  If so, you may have more success with answers to your questions on the Xilinx forums.

    https://forums.xilinx.com/t5/forums/searchpage/tab/message?advanced=false&allow_punctuation=false&q=tsn

     

    If you haven't already, you may want to register for access to the Xilinx TSV IP lounge.  This will give you access to documentation for the TSN IP.

    https://www.xilinx.com/products/intellectual-property/ef-di-25g-tsn-802-1-cm.html#documentation

     

    I suspect the issue you are seeing is that the MDIO interfaces on the PHYs are not connected to the TSN IP inside the Zynq UltraScale+ (ZU+) Programmable Logic (PL).  You will need the Vivado project to determine that.

     

    --Tom