Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General JTAG node is not accessible (on Zed Board)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 373 subscribers
  • Views 2126 views
  • Users 0 members are here
Related

JTAG node is not accessible (on Zed Board)

e14 Contributor
e14 Contributor over 10 years ago

Hello,

I was able to program the Zed board via USB-JTAG (J17) before. Today, I am unable to program the Zed board and get the following error "JTAG node is not accessible". I did re-install the Digilent cable driver from Xilinx/Vivado folder, but I still received the same error. Any help will be appreciated . Thank you.

16:26:52 INFOt: Launching XSDB server: xsdb.bat -s C:/Xilinx/SDK/2015.2/scripts/xsdb/xsdb/xsdb-server.tcl
16:26:53 INFOt: Processing command line option -hwspec C:/Projects/temp/zed-cib-ip-ver2/zed-cib-ip-ver2.sdk/ssdn_axi_v2_0_wrapper.hdf.
16:26:54 INFOt: XSDB server has started successfully.
16:26:54 INFOt: Checking for hwspec changes in the project ssdn_axi_v2_0_wrapper_hw_platform_0.
16:27:26 INFOt: Connected to target on host '127.0.0.1' and port '3121'.
16:27:26 INFOt: 'targets -set -filter {jtag_cable_name =~ "Digilent Zed 210248657980" && level==0} -index 1' command is executed.
16:27:28 ERRORt: JTAG node is not accessible

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello,

     

    If your Host PC OS is Windows 7 you might want to see if, with the USB cable connected to J17 (the JTAG interface), when you turn on the ZedBoard does your PC 'recognize' the port? When you turn on the ZedBoard you should hear a 'notification' sound and, in Windows Device Manager under "Universal Serial Bus controllers", you should see a 'USB Serial Converter' added to the list.

     

    If you do not see this I would try replacing the USB Cable and, if possible, trying a different ZedBoard as the cable or the ZedBoard are the most likely problem.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jansen0326
    0 jansen0326 over 8 years ago

    Hi,

     in Zedboard pin AB14 connect to FMC-PRSNT signal, don't assign the signal to this pin. This pin is used to control switching JTAG chain to FMC, connect signal to this pin will meet this problem when power on.

    Jansen

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer