Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Connecting customized IP to external pins on Microzed board
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 373 subscribers
  • Views 469 views
  • Users 0 members are here
Related

Connecting customized IP to external pins on Microzed board

e14 Contributor
e14 Contributor over 10 years ago

We have designed a daughter board which will go and fit into JX1 and JX2 connectors of Micorzed board. We are using some of the pins from JX1_LVDS_* and JX2_LVDS_* interfacing our daughter board to micorzed board. If I create my customized IP, how can  I connect my IP ports (rather map IP ports) to these external pins? I could not find anything in HW lab examples.

It will be a great help if somebody can let me know how can we implement it? It will be appreciated somebody can also point me to some working example.


Thanks
Kavish

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Kavish,

     

    You will need to generate a .xdc constraints file that will assign your signals to the specific pins you need. A good example of how this works would be to take a look at the master constraints file for one of our Avnet MicroZed Carrier Cards. This one is for the MicroZed FMC Carrier card:

    http://zedboard.org/sites/default/files/documentations/Z7010%20or%20Z7020%20MicroZed%20with%20MBCC-FMC-PCB-B_v2.zip

     

    You can generate something similar for your custom daughter board.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Thank you very much Gary. Can you please also let me know where to include this file during compilation of the design?

    Thanks
    Kavish

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Kavish,

     

    You can use the 'Add Sources' option in the 'Project Manager' heading in the Vivado 'Flow Navigator' pane and select 'constraints'.

     

    Perhaps it would be worth your time to go through one of the available tutorials on using the Vivado tools to implement Zynq based designs. The Avnet Zynq Speedway workshops are a good place to start:

    Developing ZynqRegistered-7000 All Programmable SoC Software (Vivado 2013.3 and 2014.4.1)

    Developing ZynqRegistered-7000 All Programmable SoC Hardware (Vivado 2013.3 and 2014.4.1)

     

    or take a look at Adam Taylor's blog:

    http://zedboard.org/content/microzed-chronicles

     

    or some of the training material on the Xilinx website.

     

    -Gary