Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design the ethernet reset
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 362 subscribers
  • Views 1064 views
  • Users 0 members are here
Related

the ethernet reset

niqingliang2003
niqingliang2003 over 8 years ago

what is the block 'ETH RESET DELAY & LVL XNSLTR' for?

what will happen if we drop 'U21/Q6'?

output of U8 is 1.8V already.

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 8 years ago

    Hi,

    Refer to the Marvel datasheet for the reasoning for the delay.

    -Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • niqingliang2003
    0 niqingliang2003 over 8 years ago in reply to jafoste4

    I found it in 4.8.1
    T(PU_RESET) requirement is 10ms, which is very bigger than T(SU_XTAL_IN) (10clks).

    I think the delay circuit is for the T(SU_XTAL_IN), but the connected ASDMB is connected to 1.8V directly without any enable signal.

    the ASDMB will use 3ms after power good.

    in other words:

    1. If we can ensure T(PU_RESET) match 10ms, we will reserve 7ms for T(SU_XTAL_IN) at least, which will match the 10clks requirement definitely.

    2. If we can not ensure the 10ms of T(PU_RESET), there is no use for discussing the 10clks of T(SU_XTAL_IN).

    So I think the delay circuit for ethernet reset is not must in microzed, isn't it?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • niqingliang2003
    0 niqingliang2003 over 8 years ago in reply to jafoste4

    I found it in 4.8.1
    T(PU_RESET) requirement is 10ms, which is very bigger than T(SU_XTAL_IN) (10clks).

    I think the delay circuit is for the T(SU_XTAL_IN), but the connected ASDMB is connected to 1.8V directly without any enable signal.

    the ASDMB will use 3ms after power good.

    in other words:

    1. If we can ensure T(PU_RESET) match 10ms, we will reserve 7ms for T(SU_XTAL_IN) at least, which will match the 10clks requirement definitely.

    2. If we can not ensure the 10ms of T(PU_RESET), there is no use for discussing the 10clks of T(SU_XTAL_IN).

    So I think the delay circuit for ethernet reset is not must in microzed, isn't it?