Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Position Microheaders Microzed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 362 subscribers
  • Views 979 views
  • Users 0 members are here
  • microheader
  • microzed
  • footprint
  • io carrier card
  • hardware guide
Related

Position Microheaders Microzed

rriem
rriem over 7 years ago

Hi,

 

I'm trying to design a custom footprint for a custom Microzed carrier card in KICAD.

I would like some help on the finding the actual position/spacing of the microheaders JX1 and JX2 on the Microzed.

 

I find 3 numbers in the Microzed documentation for this, and they all contradict:

- A spacing in the Microzed Hardware user guide is given of 1.75 inch

- A spacing in the Microzed carrier design guide (figure of I/O carrier card) is given of 1.7505 inch

- A spacing in the Microzed Hardware user guide of 0.2505 is given between the microheader and the edge of the Microzed. After some calculations, this results in a spacing between the two microheaders of 1.749 inch.

 

Can someone clear this out for me? Have I missed something?

Thank you in advance.

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 7 years ago

    Hi Robbie,

     

    I feel the top and bottom gerber layers should be published for all of the zedboards, so users can get precise measurements. Anyway, I think the difference is so slight, it is rounding error level (it is just a few hundredths of a millimeter) between 1.749 and 1,7505 inches, so may make no difference at all (the screw-holes and board edges will have greater tolerance than this).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rriem
    0 rriem over 7 years ago in reply to shabaz

    Hmm, yes I guess you are right. Maybe I'll leave it at 1.75, as the tolerances of the connector dimensions seem to be around +-0.1mm. I just got frustrated at the contradictions inside the Microzed documentation.

     

    Anyways, thank you for the quick answer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • rriem
    0 rriem over 7 years ago in reply to shabaz

    Hmm, yes I guess you are right. Maybe I'll leave it at 1.75, as the tolerances of the connector dimensions seem to be around +-0.1mm. I just got frustrated at the contradictions inside the Microzed documentation.

     

    Anyways, thank you for the quick answer.