Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Connecting I2C peripheral to EMIO Bank 13 on MicroZed Z7020
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 362 subscribers
  • Views 953 views
  • Users 0 members are here
  • microzed
  • bank 13
Related

Connecting I2C peripheral to EMIO Bank 13 on MicroZed Z7020

amybelle03
amybelle03 over 6 years ago

I would like to connect the I2C peripheral to EMIO Bank 13 pins on Microzed Z7020 board. All examples seems to leave steps out.

Has anyone accomplished this and can share the Block Design along with the Constraints?

 

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 6 years ago

    Check out Tutorial 09 of the Reference Design Section

    image

     

    MicroZed

     

    -Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • amybelle03
    0 amybelle03 over 6 years ago in reply to jafoste4

    This was not exactly what I wanted to do but did help me setup my constraints file so thanks for pointing me to this example. I wanted to use the peripheral I2C Hardware and instead of assigning I2C to MIO pins I wanted

    to set it to EMIO and use Bank 13 pins.  It did appear on the processing_system7_0 but I was confused on how to setup the constraints. It appears to have worked but I have not

    tried it on the hardware yet. This is what I ended up doing. I am showing both the AXI_iiC and the Peripheral IIC.

     

    Setting I2C Peripheral to EMIO

    image

    It now shows up on the processing_system7_0

    image

    Here is both I2cs -AXI & the Peripheral routed through the EMIO

     

    image

    Here is the constraints file I ended up with.

    # AXI iic constraints

    set_property IOSTANDARD LVCMOS33 [get_ports iic_rtl_scl_io]

    set_property IOSTANDARD LVCMOS33 [get_ports iic_rtl_sda_io]

    set_property PACKAGE_PIN G14 [get_ports iic_rtl_scl_io]

    set_property PACKAGE_PIN J15 [get_ports iic_rtl_sda_io]

    #Creating SCL CLOCK at 100 Mhz

    create_clock -name IIC_SCL_CLOCK -period 10 [get_ports iic_rtl_scl_io]

    #Input Delays

    set_input_delay -clock IIC_SCL_CLOCK -clock_fall -max 0.0 [get_ports iic_rtl_sda_io]

    set_input_delay -clock IIC_SCL_CLOCK -clock_fall -min 0.0 [get_ports iic_rtl_sda_io]

    #Output Delays

    set_output_delay -clock IIC_SCL_CLOCK -max -1.9 [get_ports iic_rtl_scl_io]

    set_output_delay -clock IIC_SCL_CLOCK -min 0.035 [get_ports iic_rtl_scl_io]

    set_output_delay -clock IIC_SCL_CLOCK -max 0.000 [get_ports iic_rtl_sda_io]

    set_output_delay -clock IIC_SCL_CLOCK -min 0.000 [get_ports iic_rtl_sda_io]

     

    #***************************************************************************

    #Peripheral IIC constraints

    set_property IOSTANDARD LVCMOS33 [get_ports IIC_0_scl_io]

    set_property IOSTANDARD LVCMOS33 [get_ports IIC_0_sda_io]

    set_property PACKAGE_PIN V11 [get_ports IIC_0_scl_io]

    set_property PACKAGE_PIN V10 [get_ports IIC_0_sda_io]

    #Creating SCL CLOCK at 100 Mhz

    create_clock -name IIC_SCL_CLOCK -period 10 [get_ports IIC_0_scl_io]

    #Input Delays

    set_input_delay -clock IIC_SCL_CLOCK -clock_fall -max 0.0 [get_ports IIC_0_sda_io]

    set_input_delay -clock IIC_SCL_CLOCK -clock_fall -min 0.0 [get_ports IIC_0_sda_io]

    #Output Delays

    set_output_delay -clock IIC_SCL_CLOCK -max -1.9 [get_ports IIC_0_scl_io]

    set_output_delay -clock IIC_SCL_CLOCK -min 0.035 [get_ports IIC_0_scl_io]

    set_output_delay -clock IIC_SCL_CLOCK -max 0.000 [get_ports IIC_0_sda_io]

    set_output_delay -clock IIC_SCL_CLOCK -min 0.000 [get_ports IIC_0_sda_io]

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • amybelle03
    0 amybelle03 over 6 years ago in reply to jafoste4

    This was not exactly what I wanted to do but did help me setup my constraints file so thanks for pointing me to this example. I wanted to use the peripheral I2C Hardware and instead of assigning I2C to MIO pins I wanted

    to set it to EMIO and use Bank 13 pins.  It did appear on the processing_system7_0 but I was confused on how to setup the constraints. It appears to have worked but I have not

    tried it on the hardware yet. This is what I ended up doing. I am showing both the AXI_iiC and the Peripheral IIC.

     

    Setting I2C Peripheral to EMIO

    image

    It now shows up on the processing_system7_0

    image

    Here is both I2cs -AXI & the Peripheral routed through the EMIO

     

    image

    Here is the constraints file I ended up with.

    # AXI iic constraints

    set_property IOSTANDARD LVCMOS33 [get_ports iic_rtl_scl_io]

    set_property IOSTANDARD LVCMOS33 [get_ports iic_rtl_sda_io]

    set_property PACKAGE_PIN G14 [get_ports iic_rtl_scl_io]

    set_property PACKAGE_PIN J15 [get_ports iic_rtl_sda_io]

    #Creating SCL CLOCK at 100 Mhz

    create_clock -name IIC_SCL_CLOCK -period 10 [get_ports iic_rtl_scl_io]

    #Input Delays

    set_input_delay -clock IIC_SCL_CLOCK -clock_fall -max 0.0 [get_ports iic_rtl_sda_io]

    set_input_delay -clock IIC_SCL_CLOCK -clock_fall -min 0.0 [get_ports iic_rtl_sda_io]

    #Output Delays

    set_output_delay -clock IIC_SCL_CLOCK -max -1.9 [get_ports iic_rtl_scl_io]

    set_output_delay -clock IIC_SCL_CLOCK -min 0.035 [get_ports iic_rtl_scl_io]

    set_output_delay -clock IIC_SCL_CLOCK -max 0.000 [get_ports iic_rtl_sda_io]

    set_output_delay -clock IIC_SCL_CLOCK -min 0.000 [get_ports iic_rtl_sda_io]

     

    #***************************************************************************

    #Peripheral IIC constraints

    set_property IOSTANDARD LVCMOS33 [get_ports IIC_0_scl_io]

    set_property IOSTANDARD LVCMOS33 [get_ports IIC_0_sda_io]

    set_property PACKAGE_PIN V11 [get_ports IIC_0_scl_io]

    set_property PACKAGE_PIN V10 [get_ports IIC_0_sda_io]

    #Creating SCL CLOCK at 100 Mhz

    create_clock -name IIC_SCL_CLOCK -period 10 [get_ports IIC_0_scl_io]

    #Input Delays

    set_input_delay -clock IIC_SCL_CLOCK -clock_fall -max 0.0 [get_ports IIC_0_sda_io]

    set_input_delay -clock IIC_SCL_CLOCK -clock_fall -min 0.0 [get_ports IIC_0_sda_io]

    #Output Delays

    set_output_delay -clock IIC_SCL_CLOCK -max -1.9 [get_ports IIC_0_scl_io]

    set_output_delay -clock IIC_SCL_CLOCK -min 0.035 [get_ports IIC_0_scl_io]

    set_output_delay -clock IIC_SCL_CLOCK -max 0.000 [get_ports IIC_0_sda_io]

    set_output_delay -clock IIC_SCL_CLOCK -min 0.000 [get_ports IIC_0_sda_io]