Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Open source MicroZed development carrier board
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 360 subscribers
  • Views 1467 views
  • Users 0 members are here
  • microzed io carrier card
  • microzed
Related

Open source MicroZed development carrier board

viktornikolov
viktornikolov over 3 years ago

Hi!

In my hobby project I want to use the MicroZed. It's a steep learning curve for me. Therefore as an intermediate "teaching case" I designed a development carrier board and published it as open source on Github: MicroZed-carrier-board.

Another motivation is the fact that the MicroZed I/O Carrier Card is no longer available for purchase.

Sure, professionals are more than capable to design their own (and better) carrier boards. My project is targeted at electronics enthusiasts. That's why I put the effort into creating the repository's Wiki.

Any constructive feedback would be welcome.

I'm not an electronics engineer but an electronics enthusiast who started with his first Arduino UNO LED blink sketch about 5 years ago.  (My background is mathematics, SW engineering and project management.)
The board does what I expect from it but I'm sure it's far from perfect. 

Viktor

image

  • Sign in to reply
  • Cancel

Top Replies

  • viktornikolov
    viktornikolov over 3 years ago in reply to dyessgg +1
    Yes, the two PMODs have the level-shifters. In my private project I need to interface with an IC running on 5 V so I put two 8-channel 3.3V/5V level-shifters on the board.
  • dyessgg
    dyessgg over 3 years ago

    No one ever gets it "perfect", especially not on the first try.  Great job!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dyessgg
    dyessgg over 3 years ago

    One question.  Two of the PMODs are labeled as 5V and the other four are labeled as 3.3V.  Is that just the power or did you also include voltage level-shifters too?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • viktornikolov
    viktornikolov over 3 years ago in reply to dyessgg

    Yes, the two PMODs have the level-shifters.
    In my private project I need to interface with an IC running on 5 V so I put two 8-channel 3.3V/5V level-shifters on the board.