Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MiniZed Hardware Design Data transfer from PL to PS DDR
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 358 subscribers
  • Views 2548 views
  • Users 0 members are here
  • zynq
  • ddr
  • dma
  • Datamover
Related

Data transfer from PL to PS DDR

Waqas
Waqas over 3 years ago

We are using MiniZed Hardware in our project. We want to move some data from PL side to PS DDR through the control of PL side. We are using AXI datamover IP to transfer data from PL to PS DDR. However, we are not able to see any data in PS DDR after PL has provided data on Streaming Interface of AXI datamover IP.

 Can anyone suggest solution to this problem??

  • Sign in to reply
  • Cancel

Top Replies

  • brianmckee
    brianmckee over 3 years ago +1
    On an Altera FPGA design I did a couple of years ago I needed to grab data from a table and load it into the PL from DRAM. I used a built in AXI interface soft macro and coded my own AXI master. Even though…
Parents
  • dyessgg
    dyessgg over 3 years ago

    How are you mapping the memory on the PS side?  It soinds like you're running into a processor cache issue.  The cpu is reading stale data from tge cache.  You either need to map the shared memory as "device memory" or do explicit cache invalidate on the shared page(s).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Waqas
    Waqas over 3 years ago in reply to dyessgg

    How can we map the shared memory as "device memory" or explicit cache invalidate on shared pages

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Waqas
    Waqas over 3 years ago in reply to dyessgg

    How can we map the shared memory as "device memory" or explicit cache invalidate on shared pages

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • dyessgg
    dyessgg over 3 years ago in reply to Waqas

    How is the PS attempting to access the "shared" memory written by the PL?  I'm mmap in your userland Linux  code.  If that is the case (which I would HIGHLY discourage), you might be able to add MAP_SHARED as the flags argument.  I'm not 100% sure it would do the correct thing to map the physical memory (DDR) into the virtual address space of the process reading the memory and make it non-cacheable.

    The proper way to do this under Linux would be to reserve the shared DDR memory with Device Tree entries (scope of which is beyond this discussion).  You would then write a kernel module to access the shared memory on behalf of the process.  It would do a cache invalidate on the page and then copy from DDR into user space.  

    If you're doing this bare metal on the A-class cores, I believe Xilinx has a cache invalidate function you can call just before you attempt to read from the shared DDR.  I don't recall off the top of my head what it is.  Look for something like XilCache....