Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MiniZed Hardware Design cannot use Tera Term to talk to miniZed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 359 subscribers
  • Views 1257 views
  • Users 0 members are here
Related

cannot use Tera Term to talk to miniZed

hlzhang
hlzhang over 7 years ago

Hi All,

 

Just got brandnew miniZed several weeks ago, and started playing with it. I followed getting started guide but came across problems now.

 

1, There was a driver installation error when connecting minized to my labtop. So I follow step 4 "In the rare circumstance that the drivers are not auto-installed, then you must manually install the driver for the FTDI FT2232H device. Visit the FTDI website and download the appropriate driver for your operating system. http://www.ftdichip.com/Drivers/VCP.htm".

After doing that, I reconnect miniZed to labtop and saw this

image

So only one USB serial converter A is installed, while converter B still does not show up. This is suspicious

 

2, So I go ahead moving to step 7 of the guide, "Set the MiniZed boot mode switch SW1 to QSPI mode (‘F’ for Flash) as shown below"

Still very confusing statement. What in the world the SW should be flipped to? Two pictures they provide are essentially contradictory to each other.

Anyway here is my current setting

image

 

3, Trea term also does not show what I want

image

No port # shows up. If I click OK, then pop up a window which says

image

 

Hope someone can help with such basic questions. Thanks for your time and attention

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 7 years ago +1
    Hi Huiliang, The images in your discussion post are not visible, although they may be visible on your browser. This is due to a bug when the discussion post is first created, the solution is to edit your…
  • ravindra488
    ravindra488 over 7 years ago +1
    Hi Huiliang, Make sure your installed proper FTDI driver in your PC. Or install the driver using the device manager. Go to the Ports(COM & LPT) and click USB Serial Port (COM20) click on the Update Driver…
Parents
  • shabaz
    shabaz over 7 years ago

    Hi Huiliang,

     

    The images in your discussion post are not visible, although they may be visible on your browser. This is due to a bug when the discussion post is first created, the solution is to edit your discussion.

    Please could you edit it (just add a character to the end of it, like a '.'), that will make the images appear so we can see them.

    See here for details:

    image

    Regarding your actual issue, the boot switches should be set as shown here:

    image

    This is described here:

    Xilinx ZYNQ - Blog 2 - Getting Code Running on the SoC

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • hlzhang
    hlzhang over 7 years ago in reply to shabaz

    very helpful. thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • hlzhang
    hlzhang over 7 years ago in reply to shabaz

    very helpful. thanks