Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design pg module led
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 359 subscribers
  • Views 1724 views
  • Users 0 members are here
Related

pg module led

tseong
tseong over 9 years ago

hi.

board : pized 7020 SOM+FMC Carrier v1

originally pg module green led light on.

but, pg module led off.

What should I do with it?

What's wrong?

 

Thank you.

  • Sign in to reply
  • Cancel

Top Replies

  • jj1989
    jj1989 over 9 years ago +1
    Only your green led light is not working? Could you give more details , please?
  • jafoste4
    jafoste4 over 9 years ago +1
    Hello Tseong, Could you please provide more information. Under what cirumstance is the led ligh on and then off? Was it initially working, and now after some time it has stopped working? PG Module acts…
  • jafoste4
    jafoste4 over 9 years ago +1
    Hello Tseong, I am still a bit confused. So did you populate the con1 connector with an FMC that you are using to monitor the data and clock? Also is your board new strait out of the box and you are having…
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Tseong,

    Could you provide me with which version of PicoZed FMC Carrier Card V1 you are using. You can find the version on the back of your carrier card printed in the silk screen. Here is an example of what to look for : MBCC-PZCC-PCB-C

    image


    If your PicoZed FMC Carrier Card V1 that you are using is the same revision as above(Rev C), you should look at the PicoZed FMC Carrier Card V1 errata.

    You can locate it at : http://zedboard.org/support/documentation/4701

    If you go to section 4.6 in the  "PicoZed FMC Carier Card Rev C Errata" document, it explains an issue with the Carrier Card when an FMC module that requires 3 amps on the 3.3V rail is plugged into the PicoZed FMC Carrier Card V1. This would explain the power isses you are experiencing with the SOM.

    The Errata also provides a workaround to this issue.

    --Josh

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tseong
    0 tseong over 9 years ago in reply to jafoste4
    I confirmed it according to your information.
     
    Here is the question.
     
    Do not you use it when the voltage is high?
     
    The board is already broken.
     
    Will the board survive by replacing the inductor?
     
    thank you -Tseong
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • tseong
    0 tseong over 9 years ago in reply to jafoste4
    I confirmed it according to your information.
     
    Here is the question.
     
    Do not you use it when the voltage is high?
     
    The board is already broken.
     
    Will the board survive by replacing the inductor?
     
    thank you -Tseong