Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design PICOZED boot up
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 356 subscribers
  • Views 1261 views
  • Users 0 members are here
Related

PICOZED boot up

jfioriglio
jfioriglio over 3 years ago

Does the Xilinx part on the board wait for the entire boot load to finish before it starts running or does it start right after BIT file is loaded?

  • Sign in to reply
  • Cancel
  • flyingbean
    flyingbean over 3 years ago

    Every FPGA architecture from Xilinx is slight or big different. For PicoZed. Zynq FPGA on PicoZED starts to run codes, such as FSBL, after the power rails finishing the predefined power-up sequence.  It is a multi-stage booting process, so Zynq FPGA starts to run codes before fully boot up. Please read Xilinx document: UG585,

    image

    There is a reset tree to control when to reset PS and PL after the booting is totally finished. FPGA source codes also can control some of the reset procedure if the user would like to change it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jfioriglio
    jfioriglio over 3 years ago

    Clarification.  When does PL start running?  After the entire load or during?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • flyingbean
    flyingbean over 3 years ago in reply to jfioriglio

    After PS release PL reset if you like to load FPGA bitstream with FSBL.elf together. There are voltage level shifter between PS and PL domain. PL reset released from PS side can make voltage level shifter work properly on PL side.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jfioriglio
    jfioriglio over 3 years ago in reply to flyingbean

    Thanks, so to start the PL after FPGA bitstream I need to release the PL reset.

    How do I go about this?  Do I use the DONE output pin or is this done thru software?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • flyingbean
    flyingbean over 3 years ago in reply to jfioriglio

    No,you don't need to do it.  Zynq FPGA already has a default mechanism to do it. If you need reset PL after the default PL reset from PS, you can  use many ways to do. One is with Linux initialization flow, which is software reset flow to reset PL once more. There is a reset pin from PS to PL if you build a FPGA project at Vivado. You can see the reset at Vivado project as this:image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jfioriglio
    jfioriglio over 3 years ago in reply to flyingbean

    Issue solved.  Bitstream is loaded and PL is configured, but because of large application load, the PS clk that I use for PL is not starting up until after complete load.  So, it seams the PL is not running.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • flyingbean
    flyingbean over 3 years ago in reply to jfioriglio

    One correction on my previous points: the level shifter between PS and PL should be enabled after FPGA bitstream loaded. So please check DONE bit for bitstream loading.

    Good to hear that you got things sorted out.