Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio Mouse and Keyboard not responding with USB OTG
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Subscribers 358 subscribers
  • Views 2502 views
  • Users 0 members are here
Related

Mouse and Keyboard not responding with USB OTG

e14 Contributor
e14 Contributor over 9 years ago

Support,

I just got my PicoZed SDR and followed the directions for startup and I cannot get my mouse or keyboard to respond.

Ideas?

Thanks,

Craig

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 9 years ago in reply to e14 Contributor +1 verified
    Just to be clear, you're plugging the USB hub into the same Micro USB to USB A socket that you plugged the USB mouse into, right? You can't use a Micro USB to USB A cable (like a phone charger style cable…
  • e14 Contributor
    e14 Contributor over 9 years ago in reply to e14 Contributor +1
    Hi, I have got this to work now. I tried a third make of hub and it worked! I have a fourth hub on order so will try that when it arrives. It seems some hubs are a bit flaky ... John
Parents
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    Are you using the FMC carrier and stock SD card?  Are you plugging it into the OTG port (not the UART port)?  I assume you're using a Micro USB to USB-A adapter, plus a USB hub to plug both the KB and mouse?

     

    Have you tried plugging just the mouse into the adapter, and if so, does the mouse light up (assuming an optical mouse)?  That would confirm that you have power and that the controller knows that it should be in host mode.

     

    I personally haven't had any problems using OTG on the FMC or my custom carrier using any of the stock SD card images.

     

    Pat

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to e14 Contributor

    Pat,

    1) Yes I am using the FMC carrier and stock SD card?

    2) Yes I am plugging into the OTG port.

    3) Yes I am using a Micro USB to USB-A adapter, plus a USB hub to plug both the KB and mouse.

    4) The only way I am able to get the mouse to light up is when the USB hub is connected.

    5) How do I know that the controller knows that it is in host mode?

    Craig

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to e14 Contributor

    Just to confirm, you're using a Micro USB to USB A female (OTG host dongle)... not a Micro USB to USB A Male (standard Micro USB cable, like you'd charge a phone with), right?

     

    I just saw this post: http://zedboard.org/content/picozed-sdr-development-kit-startup-problem , where the user was having a similar problem, caused by the incorrect cable.

     

    Pat

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to e14 Contributor

    Pat,

    I am using https://www.amazon.com/Adapter-Samusung-Android-Windows-Function/dp/B00LN3LQKQ

    Craig

    UGREEN Micro USB 2.0 OTG Cable On The Go Adapter Male Micro USB to Female USB for Samusung S7 S6 Edge S4 S3 Android or Windows Smart Phones Tablets with OTG Function 6 Inch

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to e14 Contributor

    Pat,

    I am using https://www.amazon.com/Adapter-Samusung-Android-Windows-Function/dp/B00LN3LQKQ

    Craig

    UGREEN Micro USB 2.0 OTG Cable On The Go Adapter Male Micro USB to Female USB for Samusung S7 S6 Edge S4 S3 Android or Windows Smart Phones Tablets with OTG Function 6 Inch

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to e14 Contributor

    That cable should work, though of course it's possible to have a defective cable.  If your mouse doesn't light up when plugged directly into the port using the OTG cable, I'd say either the cable is bad (isn't grounding the ID pin to tell it to be a host, bad contacts, broken wire, etc), or there's something messed up with your SOM/carrier (not seeing the ID pin, not turning on 5V, etc).  There's probably a way to echo the OTG state from Linux, but I'm not sure exactly how.

     

    Personally, I'd try another cable, or try that cable on a newer Android tablet or phone with a USB flash drive plugged in, and see if it detects it (which would tell you that the cable is good).

     

    Pat