Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio HDMI is not connected
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 26 replies
  • Subscribers 359 subscribers
  • Views 3282 views
  • Users 0 members are here
Related

HDMI is not connected

e14 Contributor
e14 Contributor over 10 years ago

Hi everyone! 

 

I have a PicoZed Development Kit and when I connect the HDMI cable the DS1 is not switch on. Other LEDs are switch good.

 

The leds that are on are:

DS8 (power) - red;

DS7 - blue;

D3 (SOM) - green;

D4 (SOM) is switch off, so Zynq PL is configured.

 

I'm connecting a monitor (VGA) through HDMI-VGA adapter. 

 

What could be the problem?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

        Dear jeckor

            my name is yangyong ,recently I meet the same problem.Did you solved the problem?Can you tell me how you solved the problem?

       thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Hi
    I didn't solved this problem. I could only to connect Linux through the terminal on the PC. HDMI does not work and there are three variants why:

    1. I use a bad VGA-HDMI adapter;
    2. HDMI on the board is defective.
     
    Besides I did not always can turn on the board (only power LED switch on).
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Hello


    I meet the same problem(only power LED DS8 switch on).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    hello


    I don't think it's the problem of the cable(VGA-HDMI dadpter).Because I use the same cable when i start  (zedboard+fmcommc3),it works fine. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Maybe it's only the my adapter is a bad.

     

    If I want to turn on the board I take my ohmmeter and short circuit something =) It's not well but it's working. Now I can work with SDR across terminal on the PC but it's not comfortable to me. I'm prefer GUI interface.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Maybe it's only the my adapter is a bad.

     

    If I want to turn on the board I take my ohmmeter and short circuit something =) It's not well but it's working. Now I can work with SDR across terminal on the PC but it's not comfortable to me. I'm prefer GUI interface.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • mbrown
    0 mbrown over 10 years ago in reply to e14 Contributor

    The process of "short circuiting" the board to get it to power up or boot has be concerned. Some of the symptoms you report sound related to another debug effort underway. I'll know more on Monday and will post back to this thread.

     

    /Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to mbrown

       hi

        why I can't start the Linux ?

       I follow the hardware setup and the demo setup.

      when I take on the S5 ,only the D8  is lighting up!

    thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    I need you help?  

    my computer can't detect the uart? What kand of drive did you setup on your computer?

    (CP210x USB-to-UART bridge driver )I had setuped on my computer.but it did'nt work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mbrown
    0 mbrown over 10 years ago in reply to e14 Contributor

    jeckor

    Are you able to try the following update of the SOM voltage supply sequencing chip (ADM1166):

    ----

    Analog Devices provides a simple Linux script executed on Zynq to download the latest ADM1166 firmware and program the SOM. You will need a networked router with DHCP capability. Follow the instructions at the wiki site listed below. Look for the section “Programming the ADM1166 Power Sequencer – Using Linux or HyperTerminal Program”.

    https://wiki.analog.com/resources/eval/user-guides/pzsdr/power-and-sequencing

    ----

    /Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to mbrown

    Thanks but now I have the more serious problem. FMC don't work. U8 is the source of problem. As I know this chip is the source of SYNC_SUPPLY signal that are needed for other stabilizers that generates 5V, 3.3V and other. Now we are trying to solve this problem. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mbrown
    0 mbrown over 10 years ago in reply to e14 Contributor

    On the FMC Carrier, do you have P8 such that VADJ = 2.5 or 3.3V?

     

    /Matt