Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
RASynBoard RAsynboard stopped working
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 15 replies
  • Subscribers 361 subscribers
  • Views 2936 views
  • Users 0 members are here
  • RASynBoard
Related

RAsynboard stopped working

balajivan1995
balajivan1995 over 2 years ago

Long story short, I was road-testing the RAsynboard and I wanted to create an activity tracker using the IMU sensor present in it. Due to the delicate nature of the board (two tiny jumpers wires on core board already started peeling away), I made sure I handled it with proper care. I strapped the board powered by a small 3.7v battery to my arm to collect data in SD card to create ML model. I am not sure, but I think due to sweat the board got shorted somewhere and stopped working. It blinks in red color for a few milli second and stops. I used prebuilt binaries for generating raw sensor values, nothing fancy. Now I can't even program it further (Created new project configuration in Renesas Programmer as well as suggested in guide). 

Since there is a dedicated forum for RAsynboard, I have decided to ask for help here. Any suggestions will be helpful. I am will gladly provide additional details if needed for clarification.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply
  • Cancel

Top Replies

  • bwilless
    bwilless over 2 years ago +1
    Sorry to hear that your board is not working. I've not seen this issue before. Does your PC recognize the Renesas Debugger hardware if your remove the J3 jumper and connect your USB-C cable to the…
  • peterfenn
    peterfenn over 2 years ago +1
    From the video plus your comments it appears that the small (1.27mm pitch) SMT 2-pin header ( J5 ) on the core board has broken-off? This damage to the PCB has likely compromised the integrity of the Boot…
  • peterfenn
    peterfenn over 2 years ago in reply to balajivan1995 +1 verified
    The last thing to possibly try here, is to reboot your PC, then re-attach the USB cable between core board and the PC... but I doubt this is an issue with your USB driver. It increasingly sounds like the…
Parents
  • bwilless
    0 bwilless over 2 years ago

    Sorry to hear that your board is not working.  I've not seen this issue before.  

    • Does your PC recognize the Renesas Debugger hardware if your remove the J3 jumper and connect your USB-C cable to the I/O board?  

    image

    Does the core board operate when separated from the I/O board? If you have an application loaded and you had flashed the models to the SPI Flash (user button > 3 seconds), the small LED between the battery connector and the USB-C connector will double flash if the application detects an inference event from the NDP120.

    • Detach the I/O board and power the core board using the USB-C connector on the core board
    • Do you see any debug from the COM port associated with the connection?
    • Maybe a better question is does the COM port associated with the USB-C connector on the core board enumerate on your PC?

    Brian

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balajivan1995
    0 balajivan1995 over 2 years ago in reply to bwilless

    Hi, I tried Peter's suggestion and soldered the J5 connectors. 

    1. Yes, I have detached the core board and powered via USB-C cable, green LED is ON. But the board is not working.

    2. No, there was no debug messages from the COM port.

    3. No, COM port did not appear in device manager at all.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • balajivan1995
    0 balajivan1995 over 2 years ago in reply to bwilless

    Hi, I tried Peter's suggestion and soldered the J5 connectors. 

    1. Yes, I have detached the core board and powered via USB-C cable, green LED is ON. But the board is not working.

    2. No, there was no debug messages from the COM port.

    3. No, COM port did not appear in device manager at all.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data