Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Zynq FSBL cannot read BOOT.bin from SD card
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 364 subscribers
  • Views 3879 views
  • Users 0 members are here
Related

Zynq FSBL cannot read BOOT.bin from SD card

e14 Contributor
e14 Contributor over 12 years ago

Hello,

I also posted my problem in the Xilinx forums (http://forums.xilinx.com/t5/Embedded-Linux/Zynq-FSBL-cannot-read-BOOT-bin-from-SD-card/m-p/522631/highlight/false), but as they couldn't help me yet and it also might be a MicroZed related problem, I'm posting it here now as well.

I have a MicroZed board with a Zynq 7020. I created a Project in Vivado and applied the board definition files provided here: http://zedboard.org/support/documentation/1519. Then I created a FSBL project in the SDK based on that hardware project. As a minimal example I generated a bootimage using the FSBL I generated and the u-boot.elf from the SD card image provided by Avnet, from the same link as above. I enabled the debug output of the FSBL and it tells me this:

Xilinx First Stage Boot Loader
Release 2014.2 Sep 22 2014-14:34:28
Devcfg driver initialized
Silicon Version 3.1
Boot mode is SD
SD: rc= 0
SD: Unable to open file BOOT.BIN: 3
SD_INIT_FAIL
FSBL Status = 0xA009

This Boot Mode Doesn't Support Fallback
In FsblHookFallback function

I am able to boot from the original BOOT.bin provided by Avnet, so neither my SD card, nor my MicroZed should be broken. As suggested in related threads, I also verified that the CD and WP pins are configured right and that the SD card clock is set to 50MHz. I tried routing the WP pin to an EMIO without any success. I also tried it with and without a .bit file. Is there anything else I could try?

Thanks,
Alain

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 11 years ago +1
    hi Alain, I'm having the exact same problem; how did you use ISE 14.7 to generate the bootimage? can you send detailed instructions? thanks
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi Alain,

      I'm just speculating, but I think the error message might be misleading.  The fact that you are able to run the FSBL indicates that the BOOTROM code was able to load and validate the Boot Header, and was able to load the FSBL to OCM and execute it.  However, when the FSBL attempts to load the next partition, it fails.   That indicates to me that the image is somehow corrupt, so I'm wondering exactly how you generated it?

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi Alain,

      I'm just speculating, but I think the error message might be misleading.  The fact that you are able to run the FSBL indicates that the BOOTROM code was able to load and validate the Boot Header, and was able to load the FSBL to OCM and execute it.  However, when the FSBL attempts to load the next partition, it fails.   That indicates to me that the image is somehow corrupt, so I'm wondering exactly how you generated it?

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    You are right. It was a problem with Vivado. I now use ISE 14.7 to generate the bootimage and that works. Somehow Vivado seems to be broken.