Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Access upper 16 MB of QSPI Flash
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 13 replies
  • Subscribers 363 subscribers
  • Views 3603 views
  • Users 0 members are here
Related

Access upper 16 MB of QSPI Flash

e14 Contributor
e14 Contributor over 13 years ago

The Zynq QSPI controller only supports 24-bit addressing (16 MB).  The Zedboard Hardware User Guide indicates the full 256 Mb capacity can be accessed via internal bank switching.

Does anybody know how to do this from Linux?  Is it possible to set up MTDs for both the lower and upper address ranges?

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Spansion has been working on validating this with the Zedboard and the S25FL-S flash that come with this board, and we have shown it is definitely possible in certain circumstances.

    In Linear mode the QSPI controller is definitely limited to 24b addressing, although it is possible to switch the bank register so this mode can access the higher banks.

    But for Linux and u-boot the QSPI IO mode is more appropriate. In our prototype u-boot code we used the bank address register to enable addressing to span >128Mb (16MB) address space. All legacy flash commands with 3B addressing are proven to work correctly for multi-IO operations, and any single-IO command can also work (the new flash commands expecting 4B address all work with QSPI so long as they are single-IO).

    In our discussions with Xilinx we've learned that the flash extended address register can be used to enable 4B address arguments for the legacy READ commands that normally expect 3B addresses; this works so long as the QSPI controller is configured to expect an extra dummy byte. This is a cleaner way to support extended addressing for single and multi-IO reads.

    Linux MTD support is a work in progress, but we're expecting to have sample code pretty soon.

    Let me know if you are interested in seeing the sample code we have so far.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Can you tell me where the detailed tutorial about how to access upper 16 MB of QSPI Flash is?Thank you very much!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Can you tell me where the detailed tutorial about how to access upper 16 MB of QSPI Flash is?Thank you very much!