Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Ultra96 V2 kernel is hanging when loading root file system
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 366 subscribers
  • Views 2012 views
  • Users 0 members are here
  • ultra96-v2
  • kernel
Related

Ultra96 V2 kernel is hanging when loading root file system

nico_n04
nico_n04 over 7 years ago

Hi,

 

I am building the kernel from source based on the https://github.com/Xilinx/linux-xlnx  kernel released by Xilinx.

I didn't find the defconfig for the ultra96 so I used the one "xilinx_zynqmp_defconfig"  which is a basic configuration for the Ultrascale+.

I am wondering if there is a particular defconfig for the Ultra96 V2 that is I need to use.

 

It is hanging when loading  root "waiting for root device /dev/mmcblk0p2". I used a uEnv.txt to load the bootargs and used root=/dev/mmcblk0p2

but I am not sure how to check what argument root should be.

 

from U-Boot, I was not sure if I needed to use the address "initrd" address with the initial RamDisk. I didn't know what to use for loading the RamDisk.

From what I read on a blog, root partition is temporally mounted on the initrd.

 

Any Ideas?

  • Sign in to reply
  • Cancel

Top Replies

  • jafoste4
    jafoste4 over 7 years ago in reply to nico_n04 +1
    Yes that is correct. -Josh
Parents
  • nico_n04
    nico_n04 over 7 years ago

    update, it is hanging due to an argument I added to the bootargs "rootwait" . It is waiting for the root=/dev/mmcblk0p2.

    I not sure what I need to set on the u-boot ,  it like it is not seen the partition where the root file is located.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jafoste4
    jafoste4 over 7 years ago in reply to nico_n04

    Hi Nicolas,

     

    Just to confirm, is the boot partition - Fat32 and the root partition formatted to EXT4?

     

    -Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • nico_n04
    nico_n04 over 7 years ago in reply to jafoste4

    Yes, boot partition is Fat32 and the root file system is in a partition formatted as EXT4.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • nico_n04
    nico_n04 over 7 years ago in reply to nico_n04

    I built u-boot from source, I am wondering if it's missing a  configuration that is not on the defconfig "avnet-Ultra96_rev1_deconfig".

    where does the header "platform-top.h" AVNET is providing suppose to go? maybe my issue is in the u-boot

    https://github.com/Avnet/petalinux/blob/master/configs/u-boot/platform-top.h.ultra96v2_sd_boot

     

    I found a similar issue for other board but it didn't help. https://forums.xilinx.com/t5/Embedded-Development-Tools/Beginners-problems-with-Ultrazed-eg/td-p/800802

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • nico_n04
    nico_n04 over 7 years ago in reply to nico_n04

    I built u-boot from source, I am wondering if it's missing a  configuration that is not on the defconfig "avnet-Ultra96_rev1_deconfig".

    where does the header "platform-top.h" AVNET is providing suppose to go? maybe my issue is in the u-boot

    https://github.com/Avnet/petalinux/blob/master/configs/u-boot/platform-top.h.ultra96v2_sd_boot

     

    I found a similar issue for other board but it didn't help. https://forums.xilinx.com/t5/Embedded-Development-Tools/Beginners-problems-with-Ultrazed-eg/td-p/800802

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • jafoste4
    jafoste4 over 7 years ago in reply to nico_n04

    Hi Nicolas,

     

    Are you opposed to reviewing the Ultra96-V1 BSP and trying to mimic this targeting the Ultra96-V2 board?

     

    If so, we will have an Ultra96-V2 BSP available in a couple weeks you could leverage to get past this problem.

     

    -Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • nico_n04
    nico_n04 over 7 years ago in reply to jafoste4

    I have figured out the issue!!

    I used the device tree configuration from Ultra96-V1 BSP. So basically I used the SDK to generate a base device tree for my PL blocks from Vivado 2018.3.

    Then I built my dtb from the dts generated plus the avnet-ultra96-rev1.dtsi . This solved the issue.

     

    I built the source u-boot with the defconfig for the ultra96 which I think it's for the version 1.  I only had to modified the bootcmd parameter it was looking for from the default configuration.

    I passed my boot cmd from the uEnv.txt file.

     

    What is the differences between the Ultra96-V1 and Ultra96-V2? I have to clean up unused configuration.

     

    thanks for your help Josh.

     

    -Nicolas

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jafoste4
    jafoste4 over 7 years ago in reply to nico_n04

    Hi Nicolas,

     

    In regards to the boards BDF, the only difference will be the DDR configurations between the V1 and V2.

     

    -Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • nico_n04
    nico_n04 over 7 years ago in reply to jafoste4

    Are those DDR configurations of the BDF for the V2 provided in github https://github.com/Avnet/bdf ?

    I used this configuration when I created my Vivado project, It contained the V2 BDF. I would assume they are the correct DDR configurations.

     

    The FSBL and PMUFW was generated by Vivado based on .hdl file that was built.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jafoste4
    jafoste4 over 7 years ago in reply to nico_n04

    Yes that is correct.

     

    image

    -Josh