Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Problem about access the output signal of vivado blocks
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 366 subscribers
  • Views 976 views
  • Users 0 members are here
Related

Problem about access the output signal of vivado blocks

pmuproject
pmuproject over 7 years ago

Hello there,

I'm current building a clock source in vivado by using the clk_wiz module. The output clock is the clk_out1 pin on the clk_wiz module. When I finish the design of vivado and export it to SDK I found that there is nothing can be used related to the clk_out1 pin. Just woundering how can I access to the clk_wiz and output the clk_out1 signal to a gpio pin in SDK?

Regards,

Han

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 7 years ago

    Hello pmuproject,

    Yes you will need to route the signal directly to the GPIO similarly to how you are showing above. Unfortunatly you will only be able to access PL GPIO, so do not use the MIO36 constraint you wrote above.

    -Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • pmuproject
    0 pmuproject over 7 years ago in reply to jafoste4

    Hi Josh,

    Thanks for your reply. In my understanding the HD and HP banks of gpio pins are PL GPIO, am I right? I just write the constraint as below:

    set_property PACKAGE_PIN D7   [get_ports {clk_out1_1              }];  # "D7.HD_GPIO_0"

    And I exported it to SDK and tried to output the clk_out1_1 signal on pin 3 which is the pin HD_GPIO0. First I tried use a Hello World code and it didn't work. Then I tried to set the direction of HD_GPIO0 to see the results. But the problem is I don't know the base address of HD_GPIO0 and the ID defined in xparameter.h. How can I output it to the HD_GPIO0 pin? Thanks for your help!

    Regards,

    Han

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • pmuproject
    0 pmuproject over 7 years ago in reply to jafoste4

    Hi Josh,

    Thanks for your reply. In my understanding the HD and HP banks of gpio pins are PL GPIO, am I right? I just write the constraint as below:

    set_property PACKAGE_PIN D7   [get_ports {clk_out1_1              }];  # "D7.HD_GPIO_0"

    And I exported it to SDK and tried to output the clk_out1_1 signal on pin 3 which is the pin HD_GPIO0. First I tried use a Hello World code and it didn't work. Then I tried to set the direction of HD_GPIO0 to see the results. But the problem is I don't know the base address of HD_GPIO0 and the ID defined in xparameter.h. How can I output it to the HD_GPIO0 pin? Thanks for your help!

    Regards,

    Han