Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Ultra 96 v2 Spontaneous Failure?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 367 subscribers
  • Views 1004 views
  • Users 0 members are here
  • ultra96-v2
  • SD card
  • mmc
Related

Ultra 96 v2 Spontaneous Failure?

mojo_jojo
mojo_jojo over 7 years ago

One of the Ultra 96 v2 boards I have worked fine for couple of hours, then suddenly it crashed while running Linux.

 

Afterwards, I always get the following on the serial port:

 

U-Boot 2018.01 (May 30 2019 - 17:43:24 +0000)

 

Model: Avnet Ultra96 Rev1

Board: Xilinx ZynqMP

I2C:   ready

DRAM:  2 GiB

EL Level:       EL2

Chip ID:        zu3eg

Watchdog: Started

MMC:   sdhci_send_command: MMC: 0 busy timeout increasing to: 200 ms.

sdhci_send_command: MMC: 0 busy timeout increasing to: 400 ms.

sdhci_send_command: MMC: 0 busy timeout increasing to: 800 ms.

sdhci_send_command: MMC: 0 busy timeout increasing to: 1600 ms.

sdhci_send_command: MMC: 0 busy timeout increasing to: 3200 ms.

sdhci_send_command: MMC: 0 busy timeout.

sdhci_send_command: MMC: 0 busy timeout.

mmc_init: -70, time 7440

mmc@ff160000 - probe failed: -70

sdhci_send_command: MMC: 0 busy timeout.

sdhci_send_command: MMC: 0 busy timeout.

mmc_init: -70, time 7414

 

sdhci_send_command: MMC: 0 busy timeout.

sdhci_send_command: MMC: 0 busy timeout.

mmc_init: -70, time 7414

** Bad device mmc 0 **

Using default environment

 

In:    serial@ff010000

Out:   serial@ff010000

Err:   serial@ff010000

Model: Avnet Ultra96 Rev1

Board: Xilinx ZynqMP

Bootmode: SD_MODE

Net:   Net Initialization Skipped

No ethernet found.

U-BOOT for ultra96v2-oob-2018-3

 

Hit any key to stop autoboot:  0

no mmc device at slot 0

 

I tried other SD cards but wasn’t able to fix the issue. The SD card that was in this board works fine on other Ultra 96 v2 boards. This appears to be a hardware failure. Could I get the board replaced by Avnet?

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 7 years ago

    Have you seen this?image

     

    I had that exact same problem with one of my development boards. It was the clock speed setting of the SD card controller (sdhci0). It was set to 25 MHz which is too slow. I changed it to 50 MHz in Vivado and generated a new HDF and then a new Petalinux  project. It then worked.

    You might be able to just change it in the device tree by adding this to system-top.dts

     

    &sdhci0 {
    clock-frequency = <25000000>;
    };

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 7 years ago

    Have you seen this?image

     

    I had that exact same problem with one of my development boards. It was the clock speed setting of the SD card controller (sdhci0). It was set to 25 MHz which is too slow. I changed it to 50 MHz in Vivado and generated a new HDF and then a new Petalinux  project. It then worked.

    You might be able to just change it in the device tree by adding this to system-top.dts

     

    &sdhci0 {
    clock-frequency = <25000000>;
    };