Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design No DP output after booting.
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 14 replies
  • Answers 2 answers
  • Subscribers 367 subscribers
  • Views 2653 views
  • Users 0 members are here
  • ultra96-v2
  • terminal
  • graphical interface
  • petalinux
Related

No DP output after booting.

riltonf
riltonf over 7 years ago

I'm using the stock linux image from the instruction manual to get the Ultra96 v2 started. I'm using the active DP to HDMI cable from amazon that was suggested. My ultra96 boots up and I see a message that it's starting to boot along with cursor. Then it goes black and there's no image. So the cable works, but the linux doesn't show a graphical nor terminal view when booted up.

I've reformatted the sd several times but still the same issue.

 

Is the only way to get an image up is to recreate my own petalinux from scratch? Or am I missing some settings first?

 

Thanks,

Ril

  • Sign in to reply
  • Cancel

Top Replies

  • riltonf
    riltonf over 6 years ago in reply to bhfletcher +1
    The new image worked. While at it I redownloaded the old image noted on the box, and it started to work. It seems my image was corrupted during downloading. I should cover my basics next time before jumping…
  • riltonf
    riltonf over 6 years ago in reply to riltonf +1
    Couldn't connect to the board, seems like the image I put on was corrupt. A fresh download fixed it.
Parents
  • bhfletcher
    0 bhfletcher over 7 years ago

    Will you please let us know which specific miniDP-to-HDMI Active Adapter that you are using?

     

    Does your monitor support one of these 3 resolutions? Do you have a different monitor that you could try?

    • 1920x1080 or
    • 1280x720

     

    If the board is booting, then re-imaging the SD Card won't help. The most common issues we see is that the Adapter isn't really Active, or the Adapter just doesn't work, or the monitor doesn't support the limited resolution.

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • riltonf
    0 riltonf over 7 years ago in reply to bhfletcher

    Cable is: https://www.amazon.com/dp/B01FM50QJC/ref=cm_sw_r_cp_ep_dp_U8xKBbXFB92BE from your response on:Ultra96-v2 mini-DP to HDMI adapter

     

    My monitor supports those resolutions as well as higher ones. Unfortunately, I don't have a spare I can try out on.

     

    I'm getting text stating the board is booting on the screen (not uart terminal), but after a few seconds it vanished and there's no signal input. The cable is an active one.

     

    What causes this discrepancy? I'd presume it should work on any screens that support the corresponding resolution, but it seems to be a hit or miss.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 7 years ago in reply to riltonf

    Yes, that is the exact cable that I use successfully all the time. I'm not sure why the discrepancy. Are you certain you are using the Ultra96-V2 image? Would you like to try the latest one that isn't posted publicly yet?

    http://avnet.me/ultra96-v2-oob-8GB

     

    Do you have the JTAG/UART Pod connected? What do you see in the terminal?

     

    If you were trying to boot an Ultra96-V1 image on Ultra96-V2, then it would fail during the boot process after configuring the hardware. That would make it appear like the display was about to work but then fail. Likewise, if you put the 16GB Delkin image on a slightly smaller SanDisk card, then that isn't always clean either, which causes the Linux boot to fail. Again, the display would start to work but then fail when the Linux boot failed.

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • riltonf
    0 riltonf over 6 years ago in reply to bhfletcher

    The new image worked. While at it I redownloaded the old image noted on the box, and it started to work. It seems my image was corrupted during downloading. I should cover my basics next time before jumping to complex solutions... Thanks for the help.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 6 years ago in reply to riltonf

    Thanks for reporting back! I'm glad to hear that Active cable is working for others as well.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 6 years ago in reply to riltonf

    Thanks for reporting back! I'm glad to hear that Active cable is working for others as well.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • riltonf
    0 riltonf over 6 years ago in reply to bhfletcher

    Can you tell me why you need an active cable? And what causes it work on some screens and not others? For example, I'd like to know if it works on: https://www.amazon.de/Raspberry-10-1-Display-Touchscreen-SunFounder/dp/B0776VNW9C/ref=sr_1_3?keywords=raspberry+pi+touch…  before I order one.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 6 years ago in reply to riltonf

    The Ultra96-V2 and V1 both drive the DisplayPort natively from the MPSoC. Therefore, it has the same limitations as any other board or system that does the same thing. You can read about this in multiple places:

    https://www.xilinx.com/support/answers/71773.html

    https://www.xilinx.com/support/answers/71774.html

    https://www.xilinx.com/support/answers/67462.html

    https://forums.xilinx.com/t5/Video/Display-Port-to-HDMI-adapters/td-p/838099

     

    Also, similar resolution limitations for the specific design, similar to the ZCU102 TRD: https://xilinx-wiki.atlassian.net/wiki/spaces/A/pages/126320678/Zynq+UltraScale+MPSoC+Base+TRD+2019.1

     

    Monitor with DisplayPort or HDMI input supporting one of the following resolutions:

    • 3840x2160 or
    • 1920x1080 or
    • 1280x720

     

    If you get one of the known-good active adapters and if your chosen display supports the resolutions shown, then it should work.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer