Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design I2C master that can provide SCK up to 1MHz?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 1 reply
  • Answers 1 answer
  • Subscribers 364 subscribers
  • Views 1116 views
  • Users 0 members are here
  • ultra96-v2
  • ultra96
Related

I2C master that can provide SCK up to 1MHz?

narrucmot
narrucmot over 5 years ago

Is it possible to implement an i2c master block in Ultra96 that can provide SCK up to 1MHz?

  • Sign in to reply
  • Cancel

Top Replies

  • narrucmot
    narrucmot over 5 years ago +2 suggested
    Both the PS I2C and PL I2C (axi_iic) peripherals for the Zynq UltraScale+ are only configurable for either 100 or 400 KHz per the I2C specification. However, there may be other 3rd party I2C IP cores available…
  • narrucmot
    0 narrucmot over 5 years ago

    Both the PS I2C and PL I2C (axi_iic) peripherals for the Zynq UltraScale+ are only configurable for either 100 or 400 KHz per the I2C specification.  However, there may be other 3rd party I2C IP cores available that can be implemented in the ZU+ PL and configured for a 1 MHz I2C SCL.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer