Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design ultra96-V2 wifi connection
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 366 subscribers
  • Views 3519 views
  • Users 0 members are here
  • ultra96v2
  • ultra96-v2
  • wifi
  • ultra96
  • connect via websever to ultra96
  • ultra -96
  • SD card
  • boot from sd
Related

ultra96-V2 wifi connection

luciaom_02
luciaom_02 over 3 years ago

Hello.

I'm using a ultra96-v2 and I'm trying to set up the wifi connection, following the guide and I'm running into some problems.
I'm reading chapter 8, "Connect to Webserver", but I can't set up the network called Ultra96-V2_<MAC_ADDRESS>.
I boot the image which is called ultra96v2_oob_2020_1_210303_8GB. But when I connect the display port, nothing comes out.

I'm also getting this error on the terminal:

ERROR:gcm_channel_status_request.cc(145)] GCM channel request failed.

Additionally, when I run the ls command it shows:

bt.sh, pmic-prog, usb_gadget_ethernet.sh, wifi.sh, wpa_supplicant.conf

But wifi.sh also runs into an error. When I run ifup wlan0 it says:

power up request for already powered up source Wifi

(full output in comment).

Can I get some help either connecting via the webserver or by setting up the wlan0 connection.

Thanks

  • Sign in to reply
  • Cancel
Parents
  • luciaom_02
    luciaom_02 over 3 years ago

    I think I'm making some progress, but still having some issues.

    When running ifdown I get the following output:

    ifdown: interface wlan0 not configured

    I have tried using ip link set wlan0 down instead. That seems to work and doesn't report any error.

    However when running either ifup wlan0 or ip link set wlan0 up, I get the following error

    [ 883.500230] power up request for already powered up source Wifi
    [ 883.506161] Device already up. request source is Wifi
    [ 883.511239] wilc_sdio mmc1:0001:1 wlan0: Failed to get mac address
    [ 883.517421] wilc_sdio mmc1:0001:1: wilc_sdio_disable_interrupt
    RTNETLINK answers: Invalid argument

    Any idea of what could be the problem?

    The other thing I have tried is to use the output of the display port. This is the option that the official guide suggests and uses a web server interface.
    However, I seem to run into the following error:

    ERROR:gcm_channel_status_request.cc(145)] GCM channel request failed.

    It appears to be related to Chromium (or maybe Selenium) but I cannot find a fix.

    Has anyone encountered the same issue and knows how to get around it?

    Thanks again

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • luciaom_02
    luciaom_02 over 3 years ago

    I think I'm making some progress, but still having some issues.

    When running ifdown I get the following output:

    ifdown: interface wlan0 not configured

    I have tried using ip link set wlan0 down instead. That seems to work and doesn't report any error.

    However when running either ifup wlan0 or ip link set wlan0 up, I get the following error

    [ 883.500230] power up request for already powered up source Wifi
    [ 883.506161] Device already up. request source is Wifi
    [ 883.511239] wilc_sdio mmc1:0001:1 wlan0: Failed to get mac address
    [ 883.517421] wilc_sdio mmc1:0001:1: wilc_sdio_disable_interrupt
    RTNETLINK answers: Invalid argument

    Any idea of what could be the problem?

    The other thing I have tried is to use the output of the display port. This is the option that the official guide suggests and uses a web server interface.
    However, I seem to run into the following error:

    ERROR:gcm_channel_status_request.cc(145)] GCM channel request failed.

    It appears to be related to Chromium (or maybe Selenium) but I cannot find a fix.

    Has anyone encountered the same issue and knows how to get around it?

    Thanks again