Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design ultra96-V2 wifi connection
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 366 subscribers
  • Views 3519 views
  • Users 0 members are here
  • ultra96v2
  • ultra96-v2
  • wifi
  • ultra96
  • connect via websever to ultra96
  • ultra -96
  • SD card
  • boot from sd
Related

ultra96-V2 wifi connection

luciaom_02
luciaom_02 over 3 years ago

Hello.

I'm using a ultra96-v2 and I'm trying to set up the wifi connection, following the guide and I'm running into some problems.
I'm reading chapter 8, "Connect to Webserver", but I can't set up the network called Ultra96-V2_<MAC_ADDRESS>.
I boot the image which is called ultra96v2_oob_2020_1_210303_8GB. But when I connect the display port, nothing comes out.

I'm also getting this error on the terminal:

ERROR:gcm_channel_status_request.cc(145)] GCM channel request failed.

Additionally, when I run the ls command it shows:

bt.sh, pmic-prog, usb_gadget_ethernet.sh, wifi.sh, wpa_supplicant.conf

But wifi.sh also runs into an error. When I run ifup wlan0 it says:

power up request for already powered up source Wifi

(full output in comment).

Can I get some help either connecting via the webserver or by setting up the wlan0 connection.

Thanks

  • Sign in to reply
  • Cancel
Parents
  • balajivan1995
    balajivan1995 over 3 years ago

    Have you tried running the .sh files?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • luciaom_02
    luciaom_02 over 3 years ago in reply to balajivan1995

    Yes, when trying to connect via wifi (using wifi.sh) I run into a problem with the configuration of the LAN. ifup wlan0 throws an error as if the device was already up (even if I set down that connection right before).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • luciaom_02
    luciaom_02 over 3 years ago in reply to balajivan1995

    Yes, when trying to connect via wifi (using wifi.sh) I run into a problem with the configuration of the LAN. ifup wlan0 throws an error as if the device was already up (even if I set down that connection right before).