Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design OOB Demo Fail - Serial Connection Gone
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 358 subscribers
  • Views 1663 views
  • Users 0 members are here
  • ultrazed
Related

OOB Demo Fail - Serial Connection Gone

Anonymous-831639
Anonymous-831639 over 6 years ago

Hi all,

 

Just opened up my new UltraZed-EV Starter Kit and followed the QuickStart Guide Instructions for getting the Out of Box Demo with a blinking light flashing.

 

Only problem is neither Terra Term nor PuTTy show any data over the connection as described, and there's no blinking light. I triple checked that all the switches were right, drivers downloaded, bit rate and other settings were correct, but I can't seem to resolve the issue. Any thoughts or tips on how to rectify the situation? Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • narrucmot
    narrucmot over 6 years ago +1
    It sounds like the UltraZed-EV SOM may not be fully seated in the connectors to the carrier board. These connectors are very stiff and it takes a lot of force to get them to fully mate. Can you try re…
  • narrucmot
    narrucmot over 6 years ago in reply to Anonymous-831639 +1
    OK, a couple of things come to mind. The UltraZed-EV will report two virtual COM ports for TeraTerm or PuTTY to use - have you tried using both of them? Only one of them will be the active STDIO UART.…
  • drozwood90
    drozwood90 over 6 years ago +1
    Hi there, Also, make certain the boot switches are set properly. If you are not careful, I have seen some customers have the inverse of what the switches SHOULD be set to. --Dan
Parents
  • narrucmot
    narrucmot over 6 years ago

    It sounds like the UltraZed-EV SOM may not be fully seated in the connectors to the carrier board.  These connectors are very stiff and it takes a lot of force to get them to fully mate.  Can you try re-seating the SOM onto the carrier?

     

    --Tom

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Anonymous-831639
    Anonymous-831639 over 6 years ago in reply to narrucmot

    Hi Tom - thanks for the tip - after inspection it did look like some of the connectors could be seated better (talk about stiff, you weren't joking!)

    However, that hasn't seemed to ameliorate the situation either. I even completely disconnected and disassembled everything and put it back together to make sure it was seated correctly. No dice.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Anonymous-831639
    Anonymous-831639 over 6 years ago in reply to narrucmot

    Hi Tom - thanks for the tip - after inspection it did look like some of the connectors could be seated better (talk about stiff, you weren't joking!)

    However, that hasn't seemed to ameliorate the situation either. I even completely disconnected and disassembled everything and put it back together to make sure it was seated correctly. No dice.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • narrucmot
    narrucmot over 6 years ago in reply to Anonymous-831639

    OK, a couple of things come to mind.  The UltraZed-EV will report two virtual COM ports for TeraTerm or PuTTY to use - have you tried using both of them?  Only one of them will be the active STDIO UART.  Also, and I apologize that this is rather rudimentary, but does the blue DONE LED turn on at power-on?  This will confirm that the PL is configured and that boot should be commencing via whatever boot method is selected.

     

    --Tom

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Anonymous-831639
    Anonymous-831639 over 6 years ago in reply to narrucmot

    Thanks for the follow up Tom!

     

    As for both ports - yes I did notice that there were two, but was unaware that only one will be active STDIO UART! Unfortunately, neither one indicates any sort of OOB demo or boot up....

     

    Sometimes "rudimentary" is what we all need = ) I for one, am not seeing the blue DONE LED firing... the red PS USER LED is on, but the PS DONE LED on the UltraZed-EV, in the bottom left corner of the board, it is not on.. thoughts on next steps? Glad you thought to ask!