Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design How to understand the swapped pins of UART0/1 on Avnet CC?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 359 subscribers
  • Views 968 views
  • Users 0 members are here
Related

How to understand the swapped pins of UART0/1 on Avnet CC?

wwqiao
wwqiao over 6 years ago

Hi,

 

According to Xilinx TRM document, UART0 uses MIO_34 (TX) and MIO_35 (RX), and UART1 uses MIO_32 (RX) and MIO_33 (TX).

 

On the Avenet Carrier Card, UART0's TX MIO_34 is connected to U16 CP2105's TXD_SCI and RX MIO_33 to U16's RXD_SCI. UART1's TX/RX pins are also swapped.

 

How to understand this design?

 

Thanks.

 

-WWQ

  • Sign in to reply
  • Cancel
Parents
  • drozwood90
    0 drozwood90 over 6 years ago

    Hi there,

     

    I'm not sure I follow.  The pins are configured in the PS by the board preset.

     

    image

    What is swapped about them?

     

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • wwqiao
    0 wwqiao over 6 years ago in reply to drozwood90

    Hi, Dan,

     

    You are right about these pins from Xilinx PS configuration. They are consistent with Xilinx TRM.

     

    The confusing comes from the notes in Avnet CC schematic and UG:
    image

     

    image

     

    Where is swizzled or swapped coming from?

     

    Thanks.

     

    -WWQ

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • wwqiao
    0 wwqiao over 6 years ago in reply to drozwood90

    Hi, Dan,

     

    You are right about these pins from Xilinx PS configuration. They are consistent with Xilinx TRM.

     

    The confusing comes from the notes in Avnet CC schematic and UG:
    image

     

    image

     

    Where is swizzled or swapped coming from?

     

    Thanks.

     

    -WWQ

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • drozwood90
    0 drozwood90 over 6 years ago in reply to wwqiao

    Hi there,

     

    I think the note is a little confusing, but was meant to explain how this is connected to the USB adapter - if you were to connect to a serial level shifter, you would likely need a different wiring (follow the manufacturers's datasheet).

    If you are implementing the serial to USB device we have, you would want to follow the way that we have designed the Carrier Card.  If you are not following what we did, you will need to implement the design as you need for your circuit per your design and the manufacturer's datasheets.

     

    I believe the point of the note was to alert you to the care needed for this, as mixing the two up will cause issues unless you have brought the signaling out the EMIO pins - which we did not.

     

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • wwqiao
    0 wwqiao over 6 years ago in reply to drozwood90

    Thanks, Dan.

     

    -WWQ