Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design UltraZed USB 3 IDS Camera Speed Issue
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 18 replies
  • Answers 6 answers
  • Subscribers 360 subscribers
  • Views 3817 views
  • Users 0 members are here
  • usb usb3 ultrazed ids ueye camera
Related

UltraZed USB 3 IDS Camera Speed Issue

jbspears
jbspears over 6 years ago

We have the UltraZed eval board (EG) and have Xilinx 2017.4 u-boot/kernel with Ubuntu 18.04 running.  USB 3 seems to be setup correctly - all USB 3 devices we've tried are recognized as USB 3.  We are connecting an IDS Ueye camera to the USB port and trying to reach a frame rate that would be approximately 1.1 Gbps throughput.  However, we are only able to get around 780 Mbps before errors start to occur in the stream transfer over USB.  We have ran the USB 3 performance test provided by Avnet with various pen/usb drives and depending on the drive and the test (fixed block/block size, etc.) sometimes to get close to 1 Gbps.  The camera works fine at the high frame rate (and even higher) on an Ubuntu desktop computer with USB 3.

 

Anyone else tried running a USB 3 camera at a high frame rate on these boards?  Or have any idea of maybe a configuration somewhere (hardware/software) that might improve the USB 3 throughput?

 

Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • jbspears
    jbspears over 6 years ago in reply to drozwood90 +1
    Thanks for the info Dan. Actually that blog article got me as far as I have gotten so far - getting a USB cable that works with the UltraZed (got the cable/adapter from Amazon). With the right cable the…
  • jbspears
    jbspears over 6 years ago in reply to drozwood90 +1 suggested
    Finally made some progress. After changing the frame size to a power of 2 (512x512) and using a powered USB hub, we are able to meet framerate (500 fps). However, we are seeing random failures with the…
Parents
  • drozwood90
    0 drozwood90 over 6 years ago

    Hi John,

     

    First, have you seen this blog article I posted?

    Solve USB 3.0 issues with this one weird trick

    Second, do you have a local XFAE you are working with?  If so, you should contact them about this issue.  Please also have them reach out to me as I can help provide some guidance to them.

     

    In the mean time, it is strange that you ask this at this time!  I just responded to another user where I explained that I had used a USB 3.0 camera with an Ultra96V2 (I realize not the same, but it is the same basic circuit).  I recall using that at high resolution, but I admit that I cannot say what the bit rate was.  Only that it was a CU30 (3.4MP) and was likely running at 1080P60.  I realize not apples to apples, but it just seemed strange two posts related to USB and video!

    https://www.e-consystems.com/ar0330-lowlight-usb-cameraboard.asp

     

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jbspears
    0 jbspears over 6 years ago in reply to drozwood90

    Thanks for the info Dan.  Actually that blog article got me as far as I have gotten so far - getting a USB cable that works with the UltraZed (got the cable/adapter from Amazon).  With the right cable the camera was recognized as a USB 3.0 device.  Since I posted this earlier today, I ran the UltraZed performance test with a USB 3 toaster and a SSD on both a Linux desktop and the UltraZed.  Both performed about the same - around 300MB/s for read and write (I need only around 130MB/s).  So that tells me the USB 3 is performing at good speeds (at least for a SSD drive anyway) and the issue may be more camera/driver related.

     

    Camera I'm using:

    https://en.ids-imaging.com/store/ui-3140cp-rev-2.html

     

    I will look through the article again for any other ideas just in case.  Thanks!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jbspears
    0 jbspears over 6 years ago in reply to drozwood90

    Finally made some progress.  After changing the frame size to a power of 2 (512x512) and using a powered USB hub, we are able to meet framerate (500 fps).  However, we are seeing random failures with the USB.  It can happen after running for 15 minutes or it can happen after running for 2 minutes.  The error messages are:

     

    [   83.289070] xhci-hcd xhci-hcd.0.auto: Stopped the command ring failed, maybe the host is dead

    [   83.313647] xhci-hcd xhci-hcd.0.auto: Abort command ring failed

    [   83.319478] xhci-hcd xhci-hcd.0.auto: HC died; cleaning up

    [   83.319527] xhci-hcd xhci-hcd.0.auto: Error while assigning device slot ID

    [   83.319531] xhci-hcd xhci-hcd.0.auto: Max number of devices this xHCI host supports is 64.

    [   83.319536] usb usb1-port1: couldn't allocate usb_device

    [   83.345402] usb 2-1: USB disconnect, device number 3

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • drozwood90
    0 drozwood90 over 6 years ago in reply to jbspears

    Hi John,

     

    Do you have a local XFAE you are working with?  If so, you should contact them about this issue.  Please also have them reach out to me as I can help provide some guidance to them.

     

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jbspears
    0 jbspears over 5 years ago in reply to drozwood90

    Update.  I think the camera works fine on the UltraZed board.  Our goal was to capture and stream frames across the network.  But that would kill the USB controller after a while.  So as a test we have an app that just captures the camera images and does nothing with them.  This will run for days without issue.  We then created an app that just streams dummy frames (totally independent of the camera app).  This app will run alone for days without issue.  But when we run them together, within an hour or so, the USB controller dies with the message below.  We cannot figure out why using the network device causes the USB controller to die.

     

    xhci-hcd xhci-hcd.0.auto: xHCI host controller not responding, assume dead

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • drozwood90
    0 drozwood90 over 5 years ago in reply to jbspears

    Hi there,

     

    Wow, what a find.  I will ping a few people, but in the mean time, is there any suspicion on power draw / issues around the USB device?  I have no proof, and this might be a red herring, but my first gut feel with this new information is, could the device be getting marginal power?  Then eventually it just...hiccups?

     

    I recall earlier you saying you resolved some issues by just adding a USB Hub.

     

    Are you also leveraging the VCU?  PL DDR memory?

    Have you checked the power estimator in Vivado?

     

    Again, not trying to side-track you, but I was just musing about this.

     

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jbspears
    0 jbspears over 5 years ago in reply to drozwood90

    I know power definitely was an issue at first.  The camera people suggested a specific ("approved") USB hub for their camera (IDS uEye).  And this solved our initial issues.  I will have our Vivado expert look into your questions.  There must be some low-level resource (power, clocks, etc.) that the network device and USB device share for this to be an issue.  I have even tried the 2020.1 tools (Avnet Petalinux, Xilinx Linux/u-boot, with Ubuntu 18.04, etc.) in hopes there was a driver fix or something, but still same issue.  We are using the UltraZed EG board.

     

    Thanks for your help!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jbspears
    0 jbspears over 5 years ago in reply to drozwood90

    FYI, new data this morning related to power.

     

    There are two processes.  The camera process just acquires frames and discards them.  The publisher process is streaming simulated images to N clients at once over the network (TCP).  Each process is totally independent of the other.

     

    I connected a USB power monitor to the camera connection.

     

    Power observations:

     

    Neither process running: 5.09V, 0.280A

    Only camera process: 5.02V, 0.544A

     

    Start camera process after publisher with 5 clients: 5.02V, 0.494A, then suddenly 5.14V, 0.137A

     

    Publisher with 1 client – best case will run for close to 18 hours

    Publisher with 2 clients - best case will run for close to 8 hours

    Publisher with 3 clients - best case will run for a couple hours

    Publisher with 4 clients - best case will run for a few minutes

    Publisher with 5 clients - best case will run for a few seconds

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ctammann
    0 ctammann over 5 years ago in reply to jbspears

    Hey John,


    Dan asked me to take a look at this as well as I'm the power expert on the team. Based on what you saw on the power monitor, it would be reasonable to assume that there could be a decent size transient when the load jumps. There is an experiment you could to try to see if it is a lack of 5V power capacity from the IO carrier causing your issue. J6 on the carrier board has a jumper shorting pins 1-2. If you remove that jumper, it removes 5V power from the generating source and leaves the USB+ rail unpowered. This feature allows both Host and Device mode operation. If this jumper is removed, you could provide 5V from an external supply to pin 2, assuming you have an external supply you could use. That would allow you to use a high current 5V supply as an experiment to see if a power limitation was causing the issue. If the design ran without issue using an external high current source, that would point pretty hard at a power limitation as the source of your problem. Let me know if you think you may be able to try this and need any assistance in setup.

    Thanks
    Chris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jbspears
    0 jbspears over 5 years ago in reply to ctammann

    Chris,

     

    Thanks for the info.  We have a power supply connected to the board and one connected to the J6 pin 2.  We still see the same behavior even with the external 5V power.  There is no current draw though since the powered USB hub is powering the camera, however without the 5V on pin 2, the USB hub itself doesn't provide enough current for the camera to fully function.  The other thing we have tried is measuring power draw when writing to the network.  With nothing running (except typical Linux processes), the current level is around 0.66A.  As we connect a client (server on the board writes fake images), the current level increases by 0.01A so after 4 clients are connected it's at 0.70A.  At this point after a few seconds/minutes, the xCHI controller dies and the kernel panics and the board locks up (all the typical LEDs are still lit though).  We then tried to get the current draw at 0.70A by something other than the network.  Using the stress Linux tool, we were able to get the draw at 0.71A and so far haven't seen the issue - of course, we haven't ran it for several hours yet (maybe an hour), but with the network test it only takes a minute or less to see the issue.  So we were struggling to figure out if the sudden current drop was causing the issue or is it a symptom of the issue.  Since the stress test hasn't caused the issue thus far, it's looking like the sudden current drop is due to the xCHI controller and camera dying.

     

    Let us know if you can think of any other tests we can perform.  Thanks for your help!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ctammann
    0 ctammann over 5 years ago in reply to jbspears

    Hey John, with the external supply have you tried connecting the camera directly to the board without the hub? Could the hub be contributing to the runtime errors?

     

    Is the USB UART getting hot? I believe it is U20 on the carrier. Forgive my ignorance, but are the data rates within the spec of this controller? https://www.silabs.com/documents/public/data-sheets/CP2105.pdf

     

    It sounds like the issue may not be directly power related, are you using a bench supply to provide 5V? Just curious if you could run the camera directly off of the carrier but still read the current draw.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jbspears
    0 jbspears over 5 years ago in reply to ctammann

    Chris, the camera is transferring about 125MB/s across USB 3.  The camera doesn't appear to draw enough current to function without the USB powered hub.  Connected directly to the board, the monitor shows 4.92V, 0.107A.

     

    While I was typing, the issue just happened.  It ran for about an hour while running the stress test (no network involved) with the board drawing 0.71A.  Same issue with the xHCI controller dying.

     

    I will look for the U20 chip and see if it's getting hot next time it crashes.  Something overheating does make sense.

     

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jbspears
    0 jbspears over 5 years ago in reply to ctammann

    Chris, the camera is transferring about 125MB/s across USB 3.  The camera doesn't appear to draw enough current to function without the USB powered hub.  Connected directly to the board, the monitor shows 4.92V, 0.107A.

     

    While I was typing, the issue just happened.  It ran for about an hour while running the stress test (no network involved) with the board drawing 0.71A.  Same issue with the xHCI controller dying.

     

    I will look for the U20 chip and see if it's getting hot next time it crashes.  Something overheating does make sense.

     

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jbspears
    0 jbspears over 5 years ago in reply to jbspears

    Just to clarify, we are connected to the USB 3 connector (J12).  Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ctammann
    0 ctammann over 5 years ago in reply to jbspears

    That's strange, so using the external supply to provide the 5V through J6 connecting the camera directly to the board doesn't work? That makes me think there is a handshake action of some kind between the hub and the camera to negotiate "asking" for more power. Otherwise using the external supply directly from the carrier should provide plenty to get the camera running.

     

    Does your EG SOM have a heatsink on the UltraScale? Based on what you've described and somewhat eliminating the 5V as a potential culprit, thermal now seems most likely if you get operation temporarily then have it drop out. I'd check the ultrascale and the hub device (really feel around for any hot components) and consider adding a desk fan or something to try and cool it down to see if operation improves. Keep us posted and I'll try to help however I can.
    Thanks
    Chris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ctammann
    0 ctammann over 5 years ago in reply to jbspears

    So as shown in this quick diagram I made, or is the Hub inbetween the carrier J12 and the camera? image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jbspears
    0 jbspears over 5 years ago in reply to ctammann

    Correct, connecting the camera directly to J12 doesn't work most of the time (it may powerup once in a while, but quickly dies when frame capture is started).

     

    We do have a heatsink/fan on the SOM.  The hub is in between the J12 and camera.

     

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • drozwood90
    0 drozwood90 over 5 years ago in reply to ctammann

    Hi John,

     

    I was just thinking, to help try to isolate what is going on, do you have a different USB device you could experiment with?  I know that so far you have had to use a USB HUB to try to isolate the camera.  I just can't seem to replicate this issue and fear that I won't be able to due to something with exactly how you have your UltraZed setup.

     

    --Dan