Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design Cypress CX4613 USB 3.0 Hub not detected
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 6 answers
  • Subscribers 358 subscribers
  • Views 2651 views
  • Users 0 members are here
  • ultrazed-ev
  • petalinux
  • cy4613
  • cypress
Related

Cypress CX4613 USB 3.0 Hub not detected

jchang_endiag
jchang_endiag over 5 years ago

We are trying to get the Cypress CY4613 HX3 USB 3.0 Shared Link Development Kit working with an Avnet UltraZed-EV Starter Kit running PetaLinux 2020.2. The UltraZed-EV SK works fine with the two other Cypress USB3 hubs, the CY4609CY4609 and CY4603CY4603. However, the CY4613CY4613 is not detected when connected to the UltraZed-EV SK. Nothing appears under lsusb or dmesg. To rule out an issue with the CY4613CY4613, it has been tested with a desktop Ubuntu system where it works fine.

What could be causing this behavior and how might we fix it? Thanks in advance.

  • Sign in to reply
  • Cancel

Top Replies

  • drozwood90
    drozwood90 over 5 years ago +1 suggested
    Hi there, Are you using a high quality USB B to USB A adapter? It is rather possible the eye is close enough that you might be bumping into a SI issue. You can check this blog which has more details about…
  • bhfletcher
    bhfletcher over 5 years ago in reply to jchang_endiag +1 suggested
    Do you have anything else plugged into the board? The only reason I ask is because I just read where Wi-Fi and USB 3.0 can interfere with each other. Making USB 3.0 Play Nice with WiFi on Ultra96-V2 B…
  • narrucmot
    narrucmot over 5 years ago +1 suggested
    Since other Cypress USB hubs work (CY4609 and CY4603 CY4603 ), it may be that the Linux device driver for the CY4613 CY4613 is missing in the kernel configuration. You could try reconfiguring the kernel…
  • drozwood90
    0 drozwood90 over 5 years ago

    Hi there,

     

    Are you using a high quality USB B to USB A adapter?

    It is rather possible the eye is close enough that you might be bumping into a SI issue.

    You can check this blog which has more details about this type of issue:
    Solve USB 3.0 issues with this one weird trick

     

    --Dan

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jchang_endiag
    0 jchang_endiag over 5 years ago in reply to drozwood90

    Hi drozwood90,

     

    Thanks for the response and sorry for the late reply; I just discovered following emails was turned off.

     

    Yes, we are using a high quality USB B to USB A adapter.  Specifically, we are using the Avnet recommended Whizz USB3 adapter.

    Any other ideas?

     

    Best Regards,

    Joe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 5 years ago in reply to jchang_endiag

    Do you have anything else plugged into the board? The only reason I ask is because I just read where Wi-Fi and USB 3.0 can interfere with each other.

    Making USB 3.0 Play Nice with WiFi on Ultra96-V2

     

    Bryan

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jchang_endiag
    0 jchang_endiag over 5 years ago in reply to bhfletcher

    Hi bhfletcher,

     

    Thanks for the response.  I have seen USB 3 disturb WiFi, though not the other way.  USB 3 disturbing WiFi seems to be the phenomenon in the article you linked as well.

     

    Regardless, there is no WiFi plugged into the board.  The only other thing plugged in is ethernet.

     

    Best Regards,

    Joe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • narrucmot
    0 narrucmot over 5 years ago

    Since other Cypress USB hubs work (CY4609 and CY4603CY4603), it may be that the Linux device driver for the CY4613CY4613 is missing in the kernel configuration.  You could try reconfiguring the kernel to examine if that device driver needs to be enabled.  If this is a new device there may not be support for it yet in the mainline Linux source tree.  In that case you may need to get the driver sources (and hopefully Yocto recipe) from Cypress and manually add them to your Linux build.

     

    --Tom

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jchang_endiag
    0 jchang_endiag over 5 years ago in reply to narrucmot

    Hi narrucmot,

     

    Thank you for the suggestion.  Cypress stated that the CY4613 "does not need a separate driver for Linux but uses the generic hub class driver provided by Libusb." (see CY4613 HX3 Hub shared link Linux Driver).

     

    Also, we decided to switch to the CY4603CY4603.  Thanks everyone for the troubleshooting suggestions.

     

    Best Regards,

    Joe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • narrucmot
    0 narrucmot over 5 years ago in reply to jchang_endiag

    Thank you for sharing the reply from Cypress.  I am glad this worked out for you in the end.

     

    Cheers,

    Tom