Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design UltraZed-EV GC LVDS Clock DC Coupling
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 358 subscribers
  • Views 957 views
  • Users 0 members are here
Related

UltraZed-EV GC LVDS Clock DC Coupling

revky
revky over 1 year ago

Hi,

I am using a SI5341 to generate a 400MHz to use as global clock on the UltraZed-EV+.

The SI5341 output buffer supply is +3V3 and the FPGA HP bank is +1V8.

The output buffer common mode voltage for this is 1.1V to 1.3V and swing is 350mV to 510mV. Due to the fact that the FPGA is on the SoM I cannot use ac coupling next to the FPGA.

My question is can I get away with DC coupling if the LVDS voltages are within range of the FPGA or should I use AC-coupling before the SoM Module?

  • Sign in to reply
  • Cancel
Parents
  • iksevas
    iksevas over 1 year ago

    You may be able to get away with the DC coupled lines if the voltages fall in range of the FPGA I/O. Ultimately you could be playing games with the voltage standard you are using in your Vivado design to make it work if it differs from the LVDS requirements of the FPGA I/O. It would be prudent if you added termination to your design that converts to the proper voltage range. Many times, it's not an ideal solution, but you could add the termination / AC coupling as close as possible to the JX connector of your Carrier Card. Give yourself options to avoid spinning the board later.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • revky
    revky over 1 year ago in reply to iksevas

    Yes, I guess this is what i have decided to go even if it is not ideal.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • revky
    revky over 1 year ago in reply to iksevas

    Yes, I guess this is what i have decided to go even if it is not ideal.