Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design No USB 3.0 on a Avnet UltraZed-EG-PCIe Board (with AES-ACC-WHIZZ-USB3 adapter)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 358 subscribers
  • Views 1185 views
  • Users 0 members are here
Related

No USB 3.0 on a Avnet UltraZed-EG-PCIe Board (with AES-ACC-WHIZZ-USB3 adapter)

weidmann
weidmann over 1 year ago

Dear Sir or Madam,

I am trying to get USB 3.0 to work on an Avnet UltraZed-EG-PCIe board.

I am using the Out of the Box Images from uz3eg_pciec_2019_1 bsp.
I have also tried the latest image from uz3eg_pciec_base_2024_1.

When I plug in a USB 3.0 device, it is only recognized as USB 2.0.

Tested devices:

    Samsung USB 3.0 SSD hard drive
    Webcam with USB 3.0
    Transcend USB 3.0 SD card reader

Output in Linux:

Webcam:
root@uz3eg-pciec-2019-1:~# lsusb -t
/:  Bus 02.Port 1: Dev 1, Class=root_hub, Driver=xhci-hcd/1p, 5000M
/:  Bus 01.Port 1: Dev 1, Class=root_hub, Driver=xhci-hcd/1p, 480M
    |__ Port 1: Dev 2, If 0, Class=Video, Driver=uvcvideo, 480M
    |__ Port 1. Dev 2, If 1, Class=Video, Driver=uvcvideo, 480M
    |__ Port 1: Dev 2, If 2, Class=Human Interface Device, Driver=usbhid, 480M

Samsung USB 3.0 SSD:
root@uz3eg-pciec-2019-1:~# lsusb -t
/:  Bus 02.Port 1: Dev 1, Class=root_hub, Driver=xhci-xhd/1p, 5000M
/:  Bus 01.Port 1: Dev 1, Class=Class=root_hub, Driver=xhci-hcd/1p, 480M
    |__ Port 1: Dev 2, If 0, Class=Mass Storage, Driver=uas, 480M

I found the following post:
community.element14.com/.../usb-3-devices-only-detected-with-usb-2-speed

I bought the AES-ACC-WHIZZ-USB3 adapter.
With this adapter, no USB device is recognized. Even USB 2.0 does not work.

Webcam:
root@uz3eg-pciec-2019-1:~# lsusb -t
/:  Bus 02.Port 1: Dev 1, Class=root_hub, Driver=xhci-hcd/1p, 5000M
/:  Bus 01.Port 1: Dev 1, Class=root_hub, Driver=xhci-hcd/1p, 480M

Samsung USB 3.0 SSD:
root@uz3eg-pciec-2019-1:~# lsusb -t
/:  Bus 02.Port 1: Dev 1, Class=root_hub, Driver=xhci-hcd/1p, 5000M
/:  Bus 01.Port 1: Dev 1, Class=root_hub, Driver=xhci-hcd/1p, 480M

If I connect a USB 2.0 extension cable to the AES-ACC-WHIZZ-USB3 adapter,
the devices (camera, HDD) are at least recognized again with USB 2.0.

I am attaching a photo of the setup.
I have not changed anything on the Out of the Box Image.
I cannot get any USB 3.0 device to work.

I am completely at a loss and need help.

With kind regards,
Sebastian

image

  • Sign in to reply
  • Cancel

Top Replies

  • iksevas
    iksevas over 1 year ago in reply to iksevas +2
    Looks like you need to review the jumpers and potentially see if the 52MHz clock for the GTR is not there from the clock synthesizer.
Parents
  • bidrohini
    bidrohini over 1 year ago

    Check if the AES-ACC-WHIZZ-USB3 adapter is connected securely. Test with high-quality USB 3.0 cables and directly connected devices if possible. USB 3.0 devices often require more power than USB 2.0. Verify that your board and adapter are powered adequately.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • bidrohini
    bidrohini over 1 year ago

    Check if the AES-ACC-WHIZZ-USB3 adapter is connected securely. Test with high-quality USB 3.0 cables and directly connected devices if possible. USB 3.0 devices often require more power than USB 2.0. Verify that your board and adapter are powered adequately.