Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design connection between CPU and PL
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 359 subscribers
  • Views 1973 views
  • Users 0 members are here
Related

connection between CPU and PL

Former Member
Former Member over 12 years ago

hi all!

My question is how can i send and recieve data through the CPU that in the board to the FPGA,when i use the Tera Term (for example) and i write the data on my PC. because i can program only the FPGA by IMPACT but i can't send data to the FPGA.

I have enother question when i write C code and running it on the CPU that in the board how can i send data to the pmod? I mean is there eny comand that can do that?

thanks

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 12 years ago +1
    In general the Zynq system talk between CPU and FPGA through Axi-bus. If you read the Axi documentation there are three types: Axi, Axi-lite and Axi-stream; each have different data rate and complexity…
  • Former Member
    Former Member over 12 years ago +1
    For sending one bit of data to pmod, there are a couple way of doing it. One is enable PS's EMIO and use constraint to connect the pin to a PMOD port. Check out Zedboard CTT (for Vivado 2013.2) chapter…
Parents
  • Former Member
    0 Former Member over 10 years ago

    I am following the online tutorial from the below link :

    https://forums.xilinx.com/xlnx/attachments/xlnx/ELINUX/8467/1/zedboard_CTT_v2013_2_130807.pdf

    I am trying to implement the setup given in the chapter 3 " embedded system design using zynq PS and PL". I am using vivado 2014.4, when when I try to modify the IP core as per their instructions , they show it has a MIO[53:0] port to which they are connecting MIO [53:0],they have shown a GPIO_I[0:0] on the zynq IP to which they connect "BTNR" and then gpio_io[0:0] theyt connect "BTNU". I am not able to implement any of these as I cannot add them on my Zynq IP,other remaining connections are well implemented.

    Is this because I am working on vivado 2014.4 which has zynq IP version of 5.5? Or am I missing something ?

    Any help will be appreciated !!

    Thanks,
    Raj

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago

    I am following the online tutorial from the below link :

    https://forums.xilinx.com/xlnx/attachments/xlnx/ELINUX/8467/1/zedboard_CTT_v2013_2_130807.pdf

    I am trying to implement the setup given in the chapter 3 " embedded system design using zynq PS and PL". I am using vivado 2014.4, when when I try to modify the IP core as per their instructions , they show it has a MIO[53:0] port to which they are connecting MIO [53:0],they have shown a GPIO_I[0:0] on the zynq IP to which they connect "BTNR" and then gpio_io[0:0] theyt connect "BTNU". I am not able to implement any of these as I cannot add them on my Zynq IP,other remaining connections are well implemented.

    Is this because I am working on vivado 2014.4 which has zynq IP version of 5.5? Or am I missing something ?

    Any help will be appreciated !!

    Thanks,
    Raj

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data