Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Zed Board
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 44 replies
  • Subscribers 360 subscribers
  • Views 4667 views
  • Users 0 members are here
Related

Zed Board

100aditya
100aditya over 9 years ago

Dear Sir/Madam,

                             In mine project i want to send data from ubuntu PC to ZedBoard using Wifi. I got one link http://zedboard.org/product/wilink-8-adaptor which talks about some kind of Wifi adpater for Micro-zed.

         Will this link and its given documents be seamlessly used with ZedBoard.

Regards

Aditya

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi Aditya,

    For a good introduction into the Zynq development environment I would suggest you go through the ZynqHW and ZynqSW Speedways.

    http://zedboard.com/course/developing-zynq%C2%AE-7000-all-programmable-soc-hardware-vivado-20133-and-201441

    http://zedboard.com/course/developing-zynq%C2%AE-7000-all-programmable-soc-software-vivado-20133-and-201441

     

    As for using the Zedboard with WILINK8 I'd suggest using PMOD's JE and JD

    Here’s the pinout for the JE and JD connectors, here is the Pinout. 

    --Josh

     

                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                               
                           

    *Predefined PS MIO peripheral function

      
       

    J3 on Rev.B WL8 Adaptor

      
       

    Signal Name

      
       

    Pmod Pin#

      
       

    ZB Pin Name

      
       

    PS            MIO Pin

      
       

    ZB Zynq pin#

      
       

    WiLink8 Pmod        Signal Name

      
       

    Zedboard Pmod-JE1           (PS Bank0)

      
       

    PMOD_D0

      
       

    1

      
       

    JE1

      
       

    MIO 13

      
       

    A6

      
       

    SDIO_D1

      
       

    PMOD_D1

      
       

    2

      
       

    JE2

      
       

    MIO 10

      
       

    G7

      
       

    SDIO_D0

      
       

    PMOD_D2

      
       

    3

      
       

    JE3

      
       

    MIO 11

      
       

    B4

      
       

    SDIO_CMD

      
       

    PMOD_D3

      
       

    4

      
       

    JE4

      
       

    MIO 12

      
       

    C5

      
       

    SDIO_CLK

      
       

    GND

      
       

    5

      
       

     

      
       

    GND

      
       

     

      
       

    GND

      
       

    VCC

      
       

    6

      
       

     

      
       

    VCC

      
       

     

      
       

    VCC

      
       

    PMOD_D4

      
       

    7

      
       

    JE7

      
       

    MIO 0

      
       

    G6

      
       

    WL_IRQ

      
       

    PMOD_D5

      
       

    8

      
       

    JE8

      
       

    MIO 9

      
       

    C4

      
       

    WLAN_EN_SOC

      
       

    PMOD_D6

      
       

    9

      
       

    JE9

      
       

    MIO 14

      
       

    B6

      
       

    SDIO_D2

      
       

    PMOD_D7

      
       

    10

      
       

    JE10

      
       

    MIO 15

      
       

    E6

      
       

    SDIO_D3

      
       

    GND

      
       

    11

      
       

     

      
       

    GND

      
       

     

      
       

    GND

      
       

    VCC

      
       

    12

      
       

     

      
       

    VCC

      
       

     

      
       

    VCC

      
                                       
       

    J1 on Rev.B WL8 Adaptor

      
       

    Signal Name

      
       

    Pmod Pin#

      
       

    ZB Pin Name

      
       

     

      
       

    ZB Zynq pin#

      
       

    WiLink8 Pmod        Signal Name

      
       

    ZedBoard    Pmod JD1                 (IO Bank13)

      
       

    PMOD_D0

      
       

    1

      
       

    JD1_P

      
       

     

      
       

    V7

      
       

    BT_HCI_CTS

      
       

    PMOD_D1

      
       

    2

      
       

    JD1_N

      
       

     

      
       

    W7

      
       

    BT_HCI_TX

      
       

    PMOD_D2

      
       

    3

      
       

    JD2_P

      
       

     

      
       

    V5

      
       

    BT_HCI_RX

      
       

    PMOD_D3

      
       

    4

      
       

    JD2_N

      
       

     

      
       

    V4

      
       

    BT_HCI_RTS

      
       

    GND

      
       

    5

      
       

     

      
       

     

      
       

     

      
       

    GND

      
       

    VCC

      
       

    6

      
       

     

      
       

     

      
       

     

      
       

    VCC

      
       

    PMOD_D4

      
       

    7

      
       

    JD3_P

      
       

     

      
       

    W6

      
       

    BT_EN_SOC

      
       

    PMOD_D5

      
       

    8

      
       

    JD3_N

      
       

     

      
       

    W5

      
       

    BT_WAKE_HOST

      
       

    PMOD_D6

      
       

    9

      
       

    JD4_P

      
       

     

      
       

    U6

      
       

    WL_RS232_TX

      
       

    PMOD_D7

      
       

    10

      
       

    JD4_N

      
       

     

      
       

    U5

      
       

    WL_RS232_RX

      
       

    GND

      
       

    11

      
       

     

      
       

     

      
       

     

      
       

    GND

      
       

    VCC

      
       

    12

      
       

     

      
       

     

      
       

     

      
       

    VCC

      
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi Aditya,

    For a good introduction into the Zynq development environment I would suggest you go through the ZynqHW and ZynqSW Speedways.

    http://zedboard.com/course/developing-zynq%C2%AE-7000-all-programmable-soc-hardware-vivado-20133-and-201441

    http://zedboard.com/course/developing-zynq%C2%AE-7000-all-programmable-soc-software-vivado-20133-and-201441

     

    As for using the Zedboard with WILINK8 I'd suggest using PMOD's JE and JD

    Here’s the pinout for the JE and JD connectors, here is the Pinout. 

    --Josh

     

                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                               
                           

    *Predefined PS MIO peripheral function

      
       

    J3 on Rev.B WL8 Adaptor

      
       

    Signal Name

      
       

    Pmod Pin#

      
       

    ZB Pin Name

      
       

    PS            MIO Pin

      
       

    ZB Zynq pin#

      
       

    WiLink8 Pmod        Signal Name

      
       

    Zedboard Pmod-JE1           (PS Bank0)

      
       

    PMOD_D0

      
       

    1

      
       

    JE1

      
       

    MIO 13

      
       

    A6

      
       

    SDIO_D1

      
       

    PMOD_D1

      
       

    2

      
       

    JE2

      
       

    MIO 10

      
       

    G7

      
       

    SDIO_D0

      
       

    PMOD_D2

      
       

    3

      
       

    JE3

      
       

    MIO 11

      
       

    B4

      
       

    SDIO_CMD

      
       

    PMOD_D3

      
       

    4

      
       

    JE4

      
       

    MIO 12

      
       

    C5

      
       

    SDIO_CLK

      
       

    GND

      
       

    5

      
       

     

      
       

    GND

      
       

     

      
       

    GND

      
       

    VCC

      
       

    6

      
       

     

      
       

    VCC

      
       

     

      
       

    VCC

      
       

    PMOD_D4

      
       

    7

      
       

    JE7

      
       

    MIO 0

      
       

    G6

      
       

    WL_IRQ

      
       

    PMOD_D5

      
       

    8

      
       

    JE8

      
       

    MIO 9

      
       

    C4

      
       

    WLAN_EN_SOC

      
       

    PMOD_D6

      
       

    9

      
       

    JE9

      
       

    MIO 14

      
       

    B6

      
       

    SDIO_D2

      
       

    PMOD_D7

      
       

    10

      
       

    JE10

      
       

    MIO 15

      
       

    E6

      
       

    SDIO_D3

      
       

    GND

      
       

    11

      
       

     

      
       

    GND

      
       

     

      
       

    GND

      
       

    VCC

      
       

    12

      
       

     

      
       

    VCC

      
       

     

      
       

    VCC

      
                                       
       

    J1 on Rev.B WL8 Adaptor

      
       

    Signal Name

      
       

    Pmod Pin#

      
       

    ZB Pin Name

      
       

     

      
       

    ZB Zynq pin#

      
       

    WiLink8 Pmod        Signal Name

      
       

    ZedBoard    Pmod JD1                 (IO Bank13)

      
       

    PMOD_D0

      
       

    1

      
       

    JD1_P

      
       

     

      
       

    V7

      
       

    BT_HCI_CTS

      
       

    PMOD_D1

      
       

    2

      
       

    JD1_N

      
       

     

      
       

    W7

      
       

    BT_HCI_TX

      
       

    PMOD_D2

      
       

    3

      
       

    JD2_P

      
       

     

      
       

    V5

      
       

    BT_HCI_RX

      
       

    PMOD_D3

      
       

    4

      
       

    JD2_N

      
       

     

      
       

    V4

      
       

    BT_HCI_RTS

      
       

    GND

      
       

    5

      
       

     

      
       

     

      
       

     

      
       

    GND

      
       

    VCC

      
       

    6

      
       

     

      
       

     

      
       

     

      
       

    VCC

      
       

    PMOD_D4

      
       

    7

      
       

    JD3_P

      
       

     

      
       

    W6

      
       

    BT_EN_SOC

      
       

    PMOD_D5

      
       

    8

      
       

    JD3_N

      
       

     

      
       

    W5

      
       

    BT_WAKE_HOST

      
       

    PMOD_D6

      
       

    9

      
       

    JD4_P

      
       

     

      
       

    U6

      
       

    WL_RS232_TX

      
       

    PMOD_D7

      
       

    10

      
       

    JD4_N

      
       

     

      
       

    U5

      
       

    WL_RS232_RX

      
       

    GND

      
       

    11

      
       

     

      
       

     

      
       

     

      
       

    GND

      
       

    VCC

      
       

    12

      
       

     

      
       

     

      
       

     

      
       

    VCC

      
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • 100aditya
    0 100aditya over 9 years ago in reply to jafoste4

    Thanks Josh..........i will look into this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100aditya
    0 100aditya over 9 years ago in reply to 100aditya

    Hi Josh,

                  I am going through the tutorials that you suggested and it seems that it is really good and helpful. I am little relaxed now. But one thing that i am afraid and i want to ask here is that.......as i am very novice to Xilinx development environment....so after doing this tutorials for the above given two links, will i be able to start mine Zed Board Project or will i need some other exposure also apart from this tutorials that you have mentioned.???....Please comment on this.

     

    Thanks 

    Aditya

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100aditya
    0 100aditya over 9 years ago in reply to 100aditya

    Hi Josh,

                      I was going through LAB 2 session of Softwrae flow link and i got some errors. Would you please help me out?? Here i am attached two snapshots which you can find out in the link :-http://zedboard.org/imce?app=ckeditor%7Csendto%40ckeditor_imceSendTo%7C&CKEditor=edit-comment-body-und-0-value&CKEditorFuncNum=2&langCode=en-gb.

    1. mine_project_snap_shot

    2.Tutorial_snap_shot

    So as per lab 2 once i imported the .xml file in SDK it show the window screen as per  "Tutorial_snap_shot" mentioned above. But I am not getting this.What i am getting is as per  mine_project_snap_shot. The two differences are :

    1- It is not able to open .xml file and showing the error that you can look into mine_project_snap_shot

    2. Z_system_wrapper.bit is not getting included in the Project window

    please tell me what is error behind this.

     

    Regards

    Aditya