Azure Sphere Starter Kit
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Azure Sphere Starter Kit
  • More
  • Cancel
Azure Sphere Starter Kit
Forum Ethernet Module Issue
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Azure Sphere Starter Kit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 54 subscribers
  • Views 1926 views
  • Users 0 members are here
  • azure sphere kit
  • azurespherech
  • azure sphere
  • azuresphkt
  • azure sphere starter kit
Related

Ethernet Module Issue

sagacr2018
sagacr2018 over 7 years ago

Hi All,

 

I connected Ethernet Module (ENC28J60) and loaded Ethernet Sample from Official GIT. When I am running the program, I am getting following error,

 

ERROR: Networking_SetInterfaceState for interface 'eth0' failed: errno=2 (No such file or directory)

 

Any clue how this can be resolved?

 

Does anyone have working ethernet code for Avnet Azure Starter Kit? 

  • Sign in to reply
  • Cancel

Top Replies

  • peterfenn
    peterfenn over 7 years ago in reply to sagacr2018 +2
    Rohit Note that while the MikroE ethernet Click board (based on ENC28J60) has pinout compatibility with the Avnet Starter Kit, the board configuration image Microsoft provides at this time (lan-enc28j60…
  • clem57
    clem57 over 7 years ago +1
    sagacr2018 I would read all the Microsoft doc . I am willing to bet the setup for the device is missing from the manifest file to permit usage of the Ethernet device. Every thing you touch on the hardware…
  • sagacr2018
    sagacr2018 over 7 years ago in reply to clem57 +1
    Thanks BB-Sphere. I researched more and its not something related to Manifest or permission. I completely missed the following step, Use of Ethernet requires a board configuration image in addition to…
Parents
  • clem57
    clem57 over 7 years ago

    sagacr2018 I would read all the Microsoft  doc. I am willing to bet the setup for the device is missing from the manifest file to permit usage of the Ethernet device. Every thing you touch on the hardware level must be registered before using.

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • sagacr2018
    sagacr2018 over 7 years ago in reply to clem57

    Thanks BB-Sphere. I researched more and its not something related to Manifest or permission. I completely missed the following step,

     

    Use of Ethernet requires a board configuration image in addition to the application image. The board configuration image contains information that the Azure Sphere Security Monitor requires to add support for Ethernet to the Azure Sphere OS. Microsoft supplies a board configuration for the Microchip ENC286J60 Ethernet chip, which is attached via SPI to ISU0 with interrupts on GPIO5. For development, we recommend the Olimex ENC28J60-H module.

    To use Ethernet on Azure Sphere, you package a board configuration image for the ENC28J60 and deploy this image package in addition to your application image package.

     

     

    Now there is another challenge! Microsoft only supplies Image with support on ISU0 and Interrupt on GPIO5 but Avnet Sphere Kit doesn't have any such combination. It has SPI on ISU1 with Interrupts on GPIO 16/17. I am trying to find out a way to create custom board configuration image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • sagacr2018
    sagacr2018 over 7 years ago in reply to clem57

    Thanks BB-Sphere. I researched more and its not something related to Manifest or permission. I completely missed the following step,

     

    Use of Ethernet requires a board configuration image in addition to the application image. The board configuration image contains information that the Azure Sphere Security Monitor requires to add support for Ethernet to the Azure Sphere OS. Microsoft supplies a board configuration for the Microchip ENC286J60 Ethernet chip, which is attached via SPI to ISU0 with interrupts on GPIO5. For development, we recommend the Olimex ENC28J60-H module.

    To use Ethernet on Azure Sphere, you package a board configuration image for the ENC28J60 and deploy this image package in addition to your application image package.

     

     

    Now there is another challenge! Microsoft only supplies Image with support on ISU0 and Interrupt on GPIO5 but Avnet Sphere Kit doesn't have any such combination. It has SPI on ISU1 with Interrupts on GPIO 16/17. I am trying to find out a way to create custom board configuration image