Azure Sphere Starter Kit
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Azure Sphere Starter Kit
  • More
  • Cancel
Azure Sphere Starter Kit
Forum contest registration app problem
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Azure Sphere Starter Kit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 53 subscribers
  • Views 1002 views
  • Users 0 members are here
Related

contest registration app problem

tosato
tosato over 7 years ago

Hi everyone,

I'm experiencing some problem with the daily sync application for the first part of the contest, I mean, the heatmap thing.

I connect my board, press the read device button, everything fine, it read my device ID, MAC and IP.

When it comes to send data to the server I got an error message saying 'URL response fail'.

 

Anyone with the same problem?

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 7 years ago in reply to tosato +2
    tosato Solution - please add 13.77.82.141 avnetagent.iotconnect.io" to c:\Windows\System32\drivers\etc\hosts This means your DNS is not resolving correctly.
  • tosato
    tosato over 7 years ago in reply to clem57 +2
    Fixed! thank you
  • immehulsolanki
    immehulsolanki over 7 years ago +2
    I have connected my kit, for the consecutive 15days i got it work correctly without any issue, But yesterday 15 sep 19 and today 16 sep 19 suddenly "URL Response error occurred". Also added "13.77.82.141avnetagent…
Parents
  • immehulsolanki
    immehulsolanki over 7 years ago

    I have connected my kit, for the consecutive 15days i got it work correctly without any issue, But yesterday 15 sep 19 and today 16 sep 19 suddenly "URL Response error occurred".
    Also added
    "13.77.82.141avnetagent.iotconnect.io" to  c:\Windows\System32\drivers\etc\hosts"

    to  my windows hosts file as suggested.

     

    but still error....

    tried DNS fulshing but still error..

     

    tried cmd ping here is the response

    "

    C:\Users\Dev>ping avnetagent.iotconnect.io

    Pinging avnetagent.iotconnect.io [13.77.82.141] with 32 bytes of data:

    Request timed out.

    Request timed out.

    Request timed out.

    Request timed out.

    Ping statistics for 13.77.82.141:

        Packets: Sent = 4, Received = 0, Lost = 4 (100% loss),

    "

    Why this problem occurred after 15days!?

    I'm sure there wont be any problem with my system,

     

    Please resolve this issue.

     

    Location: Gujarat,INDIA

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • immehulsolanki
    immehulsolanki over 7 years ago

    I have connected my kit, for the consecutive 15days i got it work correctly without any issue, But yesterday 15 sep 19 and today 16 sep 19 suddenly "URL Response error occurred".
    Also added
    "13.77.82.141avnetagent.iotconnect.io" to  c:\Windows\System32\drivers\etc\hosts"

    to  my windows hosts file as suggested.

     

    but still error....

    tried DNS fulshing but still error..

     

    tried cmd ping here is the response

    "

    C:\Users\Dev>ping avnetagent.iotconnect.io

    Pinging avnetagent.iotconnect.io [13.77.82.141] with 32 bytes of data:

    Request timed out.

    Request timed out.

    Request timed out.

    Request timed out.

    Ping statistics for 13.77.82.141:

        Packets: Sent = 4, Received = 0, Lost = 4 (100% loss),

    "

    Why this problem occurred after 15days!?

    I'm sure there wont be any problem with my system,

     

    Please resolve this issue.

     

    Location: Gujarat,INDIA

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • danzima
    danzima over 7 years ago in reply to immehulsolanki

    Hi Mehul, this is a known issue and it is being resolved now. We will extend the Connections Raffle by however many days are needed to give everyone the chance to get their entries in. Phase 1 still will close on October 27 2019, which is plenty of time to complete your Phase 1 requirement still. Thanks for the heads up!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • immehulsolanki
    immehulsolanki over 7 years ago in reply to danzima

    Thank you for the answer within a day,
    Its now working.

    Automatically, no dns flushing and hostfile stuff needed.

    Note: Ping for IP 13.77.82.141 will not work, Ignore "request timeout" message. Daily sync application will still work fine if server is ok.

    Sometimes we need to think wisely, because if device or software worked for many days and suddenly it stops then we must wait instead of fixing problem of PC/LAPTOP which was never existed.