Azure Sphere Starter Kit
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Azure Sphere Starter Kit
  • More
  • Cancel
Azure Sphere Starter Kit
Forum Azure Sphere Starter kit problem
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Azure Sphere Starter Kit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 52 subscribers
  • Views 933 views
  • Users 0 members are here
Related

Azure Sphere Starter kit problem

sahrul012
sahrul012 over 7 years ago

hi, i receive the azure sphere starter kit. for this 2 days, i've been trying to setup the device. on show device attached , the result is this

C:\Users\User\Documents>azsphere dev show-attached -v
Azure Sphere Utility version 19.5.4.53731
Copyright (C) Microsoft Corporation. All rights reserved.


Start time (UTC): Sunday, 15 September 2019 03:46:28
verbose: No response from device.
warn: Device is not responding. Could not perform version check.
verbose: No SerialSlipToTunService port is set in the registry; defaulting to 56665.
error: The device is not responding. The device may be unresponsive if it is applying an Azure Sphere operating system update; please retry in a few minutes.
verbose: No response from device.
Device is not responding. Cannot get device ID.
verbose: No SerialSlipToTunService port is set in the registry; defaulting to 56665.
IP address: 192.168.35.2
Connection path: 113
error: Command failed in 00:00:00.5222705.

 

recover command

C:\Users\User\Documents>azsphere dev recover
Starting device recovery. Please note that this may take up to 10 minutes.
Downloading recovery images...
Download complete.
Board found. Sending recovery bootloader.
Erasing flash.
Sending images.
Sending image 1 of 16.
Sending image 2 of 16.
Sending image 3 of 16.
Sending image 4 of 16.
Sending image 5 of 16.
Sending image 6 of 16.
Sending image 7 of 16.
Sending image 8 of 16.
Sending image 9 of 16.
Sending image 10 of 16.
Sending image 11 of 16.
Sending image 12 of 16.
Sending image 13 of 16.
Sending image 14 of 16.
Sending image 15 of 16.
Sending image 16 of 16.
Finished writing images; rebooting board.
error: Failed to establish communication with device after recovery. Try unplugging the device and plugging it back in, and verifying communication using 'azsphere device show-attached'. If that fails, try recovering the device again.
error: Failed to establish communication with device after recovery.
error: Command failed in 00:06:38.4735440.

 

on com21 (debug port)

[1BL] BOOT: 70900000/00000001/01000000
G=2BA374ABFFA9467CE91BA4CD2DCCF7A73AEE2CD3F879006A9837B51948754FC24F9C0B72454B913345AA202A8CCB4767D1FA898E89A5E4CE62C8662B2DF6E29F
[1BL] !! ERROR: capability image is not for this device
D=e49ed334e06f4bae28b0b715a6d7d2d1c554a92f904b1677bcf0e1d41727edbca19a7651ee878476d07fa0eb2c65b7d360b931f33c599188df82bb4ea6656253,N=fc93f96fe2ad574994876b92dc2cd114e6687f08ca283bb9866a069a8ee0e5b6
[PLUTON] Logging initialized
[PLUTON] Booting application core

 

does this mean the board faulty? or the image flashed through recover is wrong.

i cant create a tenant, check device id, check version of os installed. i've been trying to use another cable, same result.

  • Sign in to reply
  • Cancel

Top Replies

  • sahrul012
    sahrul012 over 7 years ago +1
    hi i have successfully get the device id. idk wat happen. but i can use the device now
Parents
  • peterfenn
    peterfenn over 7 years ago

    Sahrul

     

    Please read the section on TAP-Windows adapter at:
    https://docs.microsoft.com/en-us/azure-sphere/install/troubleshoot-installation

     

    Notes:
    1) Your "Recovery" and "Debug" serial interfaces are working correctly. This verifies that the FTDI drivers are installed correctly

    2) If you have a VPN client network adapter running (eg. Cisco AnyConnect Secure Mobility Client Connection) this could be your problem.
    If this is the case, disable this VPN "adapter" an retest the SDK commandline communication with Azure Sphere

     

    -Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • peterfenn
    peterfenn over 7 years ago

    Sahrul

     

    Please read the section on TAP-Windows adapter at:
    https://docs.microsoft.com/en-us/azure-sphere/install/troubleshoot-installation

     

    Notes:
    1) Your "Recovery" and "Debug" serial interfaces are working correctly. This verifies that the FTDI drivers are installed correctly

    2) If you have a VPN client network adapter running (eg. Cisco AnyConnect Secure Mobility Client Connection) this could be your problem.
    If this is the case, disable this VPN "adapter" an retest the SDK commandline communication with Azure Sphere

     

    -Peter