Azure Sphere Starter Kit
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Azure Sphere Starter Kit
  • More
  • Cancel
Azure Sphere Starter Kit
Forum Sideload problems
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Azure Sphere Starter Kit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 51 subscribers
  • Views 1402 views
  • Users 0 members are here
Related

Sideload problems

wizio
wizio over 6 years ago

Nice !? .... tested on two PC

 

{"Name":"APP_AZURE","Capabilities":{"SystemTime":true,"Uart":["ISU0"],"SpiMaster":[],"I2cMaster":[],"Gpio":[],"AllowedConnections":[],"WifiConfig":true},"CmdArgs":[],"EntryPoint":"/bin/app","SchemaVersion":1,"ComponentId":"1640B7FB-4924-46DF-AE72-38998065455B","TargetApplicationRuntimeVersion":2,"TargetBetaApis":"Beta1905"}

 

azsphere device sideload deploy --imagepackage PATH/app.image --verbose

 

Azure Sphere Utility version 19.5.4.53731

Copyright (C) Microsoft Corporation. All rights reserved.

Start time (UTC): Thursday, 10 October 2019 07:31:03

Deploying 'PATH\app.image' to the attached device.

verbose: No SerialSlipToTunService port is set in the registry; defaulting to 56665.

error: This app targets Beta APIs that may no longer be supported by this device. The app may fail to start or otherwise behave unexpectedly. Please upgrade your app

to target the API sets that this device supports. Use the '--force' flag to force this operation.

error: Command failed in 00:00:02.1843316.

 

After recover:

Azure Sphere Utility version 19.5.4.53731  ( there is no new versions ) same error

  • Sign in to reply
  • Cancel
Parents
  • peterfenn
    peterfenn over 6 years ago

    Georgi

     

    If your Azure Sphere OS has updated to 19.09, then you also need to install the new 19.09 SDK and rebuild the application.

    https://docs.microsoft.com/en-us/azure-sphere/resources/release-notes-1909

     

    In Visual Studio you will need to adjust the target API Set that's used in the build (previous 2+Beta1905 APIs are no longer applicable)

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • peterfenn
    peterfenn over 6 years ago in reply to peterfenn

    More info on this topic is available here:
    https://docs.microsoft.com/en-us/azure-sphere/app-development/use-beta#target-api-sets-arv-and-sysroots

    PS: Beta APIs can change. Builds with an older SDK that only made use of production APIs are not affected by OS updates  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • peterfenn
    peterfenn over 6 years ago in reply to peterfenn

    More info on this topic is available here:
    https://docs.microsoft.com/en-us/azure-sphere/app-development/use-beta#target-api-sets-arv-and-sysroots

    PS: Beta APIs can change. Builds with an older SDK that only made use of production APIs are not affected by OS updates  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • peterfenn
    peterfenn over 6 years ago in reply to peterfenn

    Latest 19.09 SDK reports as follows:

     

    Azure Sphere Utility version 19.9.5.42479

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • peterfenn
    peterfenn over 6 years ago in reply to peterfenn

    To see the SDK version:
    azsphere show-version

     

    To see the OS version:

    azsphere device show-ota-status

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wizio
    wizio over 6 years ago in reply to peterfenn

    I haven't changed anything.

    This came as a surprise today...

    I find workaround for now: pack image as --sysroot 2 ( but is compiled with Beta1905 )  no errors, work ....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wizio
    wizio over 6 years ago in reply to peterfenn
    azsphere show-version                                                                            
    19.05                                                                                               
    Command completed successfully in 00:00:00.1611137.                                                

    BTW: I test on Windows 10, 8 and 7 too image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wizio
    wizio over 6 years ago in reply to peterfenn

    so 19.09 not work with Beta1905 ??

    $ ./azsphere device show-ota-status                                                                  
    Your device is running Azure Sphere OS version 19.09.                                               
    The Azure Sphere Security Service is targeting this device with Azure Sphere OS version 19.09.      
    Your device has the expected version of the Azure Sphere OS: 19.09.                                 
    Command completed successfully in 00:00:04.9280898.