Azure Sphere Starter Kit
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Azure Sphere Starter Kit
  • More
  • Cancel
Azure Sphere Starter Kit
Forum Using MikroElektronika Libraries with Azure Sphere MT3620 Kit
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Azure Sphere Starter Kit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 4 answers
  • Subscribers 54 subscribers
  • Views 1529 views
  • Users 0 members are here
  • azure sphere kit
  • azurespherech
  • azure sphere
Related

Using MikroElektronika Libraries with Azure Sphere MT3620 Kit

rsc
rsc over 7 years ago

Does anyone know how to include a MikroElectronika library package file (.mpkg) in a Visual Studio project?

I have some click boards I'd like to use in my project.

 

I can extract the files from the library using the MikroE Package Manager and try and add them manually I guess.

 

Scott

  • Sign in to reply
  • Cancel

Top Replies

  • peterfenn
    peterfenn over 7 years ago in reply to Fred27 +4 suggested
    David [+others on this thread] Please note the following two repositories for Click board driver code already ported for use with the Avnet Azure Sphere Starter Kit Repo for click boards already supported…
  • peterfenn
    peterfenn over 7 years ago +3 suggested
    For some practical guidance on using Click boards with the Azure Sphere Starter Kit, I recommend reading the following blog article: http://avnet.me/mt3620-click -Peter
  • cswiger
    cswiger over 7 years ago +2
    I would like to use a Click board I already have, the Nano GPS https://www.mikroe.com/nano-gps-click From a little checking that should be straightforward UART on tx/rx of the socket. I tried the https…
Parents
  • Fred27
    0 Fred27 over 7 years ago

    I was thinking about devices where there wasn't already example code for the MT3620 - such as the PN7120-based NFC click. On that case the mpkg files are not much use and it seems like it would be easiest to start from sample C code for another processor.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Fred27
    0 Fred27 over 7 years ago

    I was thinking about devices where there wasn't already example code for the MT3620 - such as the PN7120-based NFC click. On that case the mpkg files are not much use and it seems like it would be easiest to start from sample C code for another processor.