Azure Sphere Starter Kit
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Azure Sphere Starter Kit
  • More
  • Cancel
Azure Sphere Starter Kit
Forum Can you enter both contests?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Azure Sphere Starter Kit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 9 answers
  • Subscribers 54 subscribers
  • Views 1691 views
  • Users 0 members are here
Related

Can you enter both contests?

elviswolcott
elviswolcott over 7 years ago

Are we allowed to enter a project into both the Hackster.io and element14 challenges/contests?

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 7 years ago +4 suggested
    You can definitely participate in both contests if you have a separate device for each contest. I don't know if it is possible with one device - you would at least need to satisfy both phase 1 synch periods…
  • danzima
    danzima over 7 years ago +3 suggested
    Hi Elvis! Douglas has it correct below: you can join both contests, but your submissions to both MUST be unique. It is a standard term of our Design Challenges that your build must be unique to that challenge…
  • danzima
    danzima over 7 years ago in reply to elviswolcott +3 suggested
    Hi Elvis, you certainly could enter with one device! But we understand if it's easier to do two builds with two kits, so if you request a second (if available) and are not abusing the system we are fine…
Parents
  • dougw
    0 dougw over 7 years ago

    You can definitely participate in both contests if you have a separate device for each contest.

    I don't know if it is possible with one device - you would at least need to satisfy both phase 1 synch periods without overlap (ie synch for 45 days instead of 15 or 30) and create two different IoT applications for phase 2. However since one objective is to test maximum simultaneous access, and 1 device cannot look like 2 devices, it would be more compliant to have 2 devices.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • dougw
    0 dougw over 7 years ago

    You can definitely participate in both contests if you have a separate device for each contest.

    I don't know if it is possible with one device - you would at least need to satisfy both phase 1 synch periods without overlap (ie synch for 45 days instead of 15 or 30) and create two different IoT applications for phase 2. However since one objective is to test maximum simultaneous access, and 1 device cannot look like 2 devices, it would be more compliant to have 2 devices.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer