Azure Sphere Starter Kit
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Azure Sphere Starter Kit
  • More
  • Cancel
Azure Sphere Starter Kit
Forum Azure Sphere can't see iPhone Hot Spot
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Azure Sphere Starter Kit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 4 answers
  • Subscribers 52 subscribers
  • Views 1669 views
  • Users 0 members are here
  • wifi
  • azurespherech
  • azure sphere
  • connection problem
  • azuresphkt
  • azure sphere starter kit
  • ios
Related

Azure Sphere can't see iPhone Hot Spot

techyg
techyg over 7 years ago

I was able to get through all the steps of the Azure Sphere setup, up until I need to connect to wifi to get the device updated. I am in a locked down corporate environment, and need to use a phone hot spot for development. I am on the latest version of iOS (12.4).

 

I have tried adding my hot spot SSID using the "azsphere device wifi add --ssid <yourSSID> --key <yourNetworkKey>"

 

Unfortunately, this does not seem to work, and it doesn't see my iOS hot spot. I checked by running "azsphere device wifi scan" and it does see many other ssid's (that I don't have access to) so I know the wifi is working. I also confirmed it added my ssid by using the azsphere device wifi list command. I do see the SSID from my PC, and am able to connect to it, so I know the hotspot is working.

 

Based on some google searching, I believe the iOS hotspot is using WPA 2 Personal.  According to the MSDN documentation section "Configure Networking" it says that you need WPA/WPA2. Can anyone confirm that Azure Sphere should be able to use this? Or is there any step I am missing?

  • Sign in to reply
  • Cancel

Top Replies

  • gcsimmonsjr
    gcsimmonsjr over 6 years ago in reply to clem57 +2
    I have an iPhone XR running IOS 13.2.2 and for the LIFE of me, I cannot get my Sphere to connect to it's hotspot. I updated my SDK to 19.10 AND the device to 19.10. No Joy. Is there a special incantation…
  • kmikemoo
    kmikemoo over 7 years ago +1 suggested
    The Azure Sphere will work with an iPhone IOS 12.4. I just checked it with my iPhone. I also did check-ins for a week from the road using it. After adding my hotspot, I did need to enable it. After ADD…
  • clem57
    clem57 over 7 years ago +1
    azsphere device wifi list Shows what items are added. Pay close attention to enabled or disabled. Use this if disabled replace # with the number in the list command: azsphere device wifi enable -i # techyg…
Parents
  • kmikemoo
    0 kmikemoo over 7 years ago

    The Azure Sphere will work with an iPhone IOS 12.4.  I just checked it with my iPhone.  I also did check-ins for a week from the road using it.

     

    After adding my hotspot, I did need to enable it.  After ADD, it was disabled by default.  By doing the azsphere device wifi scan, my phone's "connected" banner pulses to tell me that it's at least pinging the phone.

     

    Hope this helps.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • kmikemoo
    0 kmikemoo over 7 years ago

    The Azure Sphere will work with an iPhone IOS 12.4.  I just checked it with my iPhone.  I also did check-ins for a week from the road using it.

     

    After adding my hotspot, I did need to enable it.  After ADD, it was disabled by default.  By doing the azsphere device wifi scan, my phone's "connected" banner pulses to tell me that it's at least pinging the phone.

     

    Hope this helps.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer