Azure Sphere Starter Kit
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Azure Sphere Starter Kit
  • More
  • Cancel
Azure Sphere Starter Kit
Forum Azure Sphere – How to generate Leaf certificate?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Azure Sphere Starter Kit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 52 subscribers
  • Views 785 views
  • Users 0 members are here
  • azure sphere kit
  • azurespherech
  • azure sphere
  • azuresphkt
  • azure sphere starter kit
Related

Azure Sphere – How to generate Leaf certificate?

frelfrel
frelfrel over 7 years ago

Azure Sphere – How to generate Leaf certificate?

 

It is easy to connect first device to IoT Central. There is step by step. By I want to connect second Azure Sphere device to IoT Central. It is added automatically, just because it is in Azure Sphere Tenant.

 

But I need to add generate Leaf Certificate for that device. How to do it step by step?

  • Sign in to reply
  • Cancel

Top Replies

  • bwilless
    bwilless over 7 years ago +1 suggested
    The way to use a Device Provisioning Service (DPS) to connect devices to an IoT Central application is documented here: https://docs.microsoft.com/en-us/azure-sphere/app-development/setup-iot-central …
  • danzima
    0 danzima over 7 years ago

    Hi peterfenn , any ideas on this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 7 years ago

    frelfrel  wrote:

     

    Azure Sphere – How to generate Leaf certificate?

     

    It is easy to connect first device to IoT Central. There is step by step. By I want to connect second Azure Sphere device to IoT Central. It is added automatically, just because it is in Azure Sphere Tenant.

     

    But I need to add generate Leaf Certificate for that device. How to do it step by step?

    Potentially impacted: Devices using a connection stack other than the connection stack provided in an Azure IoT SDK. Specifically, connection logic that pins the leaf certificate will experience TLS connection failures after the rollover if not updated. Our recommendation is to pin the root certificates as they renew less frequently.

     

    Why you not following this recommendation?

     

    BTW, did you see this which uses the intermediate cert?

    Here is another going to use a fake device having troubles.

    Another log into the wilderness of Microsoft docs.

     

    Note a temporary solution (good for 30 days only) is this one. But not for production. Sorry for the pointers, but that is the only was to cover the confusion.

     

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bwilless
    0 bwilless over 7 years ago

    The way to use a Device Provisioning Service (DPS) to connect devices to an IoT Central application is documented here:  https://docs.microsoft.com/en-us/azure-sphere/app-development/setup-iot-central.  This will allow you to connect millions of devices to your application and all the devices can use the same application build.

     

    The Avnet OOB examples use connection strings and are not setup to use DPS.  You can look at the Microsoft examples on GitHub which all use DPS (I'm pretty sure).

     

    If you are using the Avnet OOB examples, you can just manually create a second device and connection string, like you did with the first device.  This will require that both devices use different application builds, each with the correct connection string.

     

    Brian

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • clem57
    0 clem57 over 7 years ago in reply to bwilless

    I will have to explore this doc. Thanks bwilless

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • frelfrel
    0 frelfrel over 7 years ago in reply to clem57

    Anyway how to assign to device existing root certificate?